Automotive Equipment News
New Automotive Equipment News Release
 
Automotive Engineering Exposition2006
Mitsubishi Electric exhibited the Automotive Engineering Exposition 2006.
Thank you very much for visiting our booth.
Mitsubishi Electric Corporation Booth Guide  Booth no.47
map
Information&Entertainment
1 OMNICAR
Car multimedia system



2 HDD car navigation system CU-H9700
This system is installed with a new generation operating system that manipulates it without seeing it.
3 In-vehicle Terrestrial Digital TV Tuner
Mitsubishi developed a new receiving algorithm for Terrestrial Digital TV broadcasting, called "D3A engine".
4 ITS On-board Unit compatible with Smart-way
Using the DSRC technologies accumulated in ETC, we are developing an on-board unit for use in the ITS service that the Ministry of Land, Infrastructure and Transportation will open up in 2007.
5 ETC Onboard Unit
Slim and compact.
Environment
6 Integrated Intelligent Power Drive Unit
A unique new-generation power device and consolidated power inverter increase efficiency and make the unit more compact.
7 Electric Power Steering(Motor and Controller)
Our brushless EPS motors with higher power and lower inertia EPS can be installed also in medium and oversized vehicles.
8 Stable Steering Assistance(Torque-controlled Active Steering)
Even if on a slippery road surface, the EPS-ECU's Stable Steering Assistance function detects front tire slippage at an early stage. With such steering assistance, the driver can avoid dangerous situations, such as a spin, making stable driving possible.
Safety&Security
9 Millimeter-wave Radar
A world-class system with a wider detection range of 1-200m for passenger vehicles.
10 Lane Recognition Camera
Accurately recognizes the lane even in locations where brightness rapidly changes,such as tunnel entrances or exits.