Communication Systems Installations
DCME/IP-CME
The EAC Upgrade was Mitsubishi Electric's first upgrade undertaken as the prime contractor. Despite being on an extremely tight timescale, Mitsubishi Electric completed the EAC upgrade ahead of the contracted schedule due to a combination of problem-free manufacturing and well-organized on-site installation teams. Commissioning was particularly trouble-free, with the new equipment performing extremely reliably, and all transmission performance specifications were either met or considerably exceeded.


Optical Submarine Cable Network
NO Project Completion Length Capacity (MAX)
1 TPC-5CN Mar 1995 / Oct 1996 25,000km 5G-1
2 APCN Sep 1996 12,000km 5G-1
3 MOC June 1997 11,000km 5G-1
4 FLAG Sep 1997 27,000km 5G-1
5 SEA-ME-WE-3 Dec 1998 30,000km 2.5G-8
6 JIH Mar 1999 10,300km 2.5G-24
7 China-US Dec 1999 30,500km 2.5G-8
8 PC-1 Jan 2000 20,900km 10G-16
9 Japan-US Jul 2001 22,000km 10G-16
10 TAT14 Apr 2001 15,300km 10G-16
11 EAC Dec 2000 / Jun 2001 11,600km 10G-64
12 C2C Oct 2001
13 SEA-ME-WE-3Upgrade Dec 2002
14 JIH Upgrade 2004 / 2005 / 2006
15 MOC Upgrade 2004 / 2007
16 EAC Upgrade Dec 2006

TOP