Installation

School

Ohara Bookkeeping Special School, Nagoya Campus

High-speed Hand Dryer Slim Type makes a clean sweep of all paper waste

"The decision to introduce the High-speed Hand Dryer was based the use of that same model at a separate campus within our school group. The conventional paper towels used in our student restrooms were creating a major mess, and we realized that a cleaner environment was needed. Putting the High-speed Hand Dryer Slim Type into use also enhanced the restroom ambience, furnishing a nice touch of luxury. The no-contact drying function has also been a big hit with our students for its simplicity and handy use."



Factors behind the decision to use the High-speed Hand Dryer:


1. Improved student restroom convenience
2. Improved school image
3. Improved paper waste countermeasure and restroom space comfort


Background to Installation Existing facility
Previous drying system Paper towels
Installation sites Student restrooms
Number installed 12 units
Adogawa-cho Combined School Foodservice Facility

A hit with clients. Reduces maintenance costs. Friendly to the environment.

"We're especially careful here about hygiene standards. All employees are required to wash their hands an average of 7-8 times a day. So the High-speed Hand Dryer, which dries hands quickly, is extremely popular among our employees. Switching from paper towels to the High-speed Hand Dryer offers other advantages, too; for example, eliminating paper waste and the need to restock paper towels."



Factors behind the decision to use the High-speed Hand Dryer:


1. Hygienic no-contact drying
2. Faster drying with dual-jet airflow
3. No paper waste


Background to Installation New building
Previous drying system Paper towels
Installation sites Hand-washing facilities
Number installed 28 units
High-speed Hand Dryer
High-speed Hand Dryer’s many benefits make it suitable for a wide range of environments.