Multimedia Projectors Technology
Ease of Operation
Operating a projector has never been easier. Mitsubishi has incorporated a number of operator assistance technologies,such as placing a laser pointer and data source control buttons in the remote control unit, equipping the projector with a USB port and giving the operator the choice of what language the operation menu is to be displayed in.
Anti-Theft Alarm
The ceiling-use projector is equipped with a built-in anti-theft alarm. Once the projector is installed and the alarm is set, any unauthorized attempt to move the unit will cause the alarm to sound.
PAGE TOP PAGE TOP
Anti-Theft Password

This projector is equipped with the password function that is designed for prevention of theft and wrong operation by children and restriction on operation by other than specified users. The password function has three modes as follows:

DISPLAY INPUT
When the projector is turned on, the startup screen (or splash screen) will appear and stay on the screen until the password is entered. When the password is entered, the LOCK OK startup screen will switch to the regular operation screen.

MENU ACCESS
All the buttons except for the POWER button on the projector are disabled. (The buttons on the remote control are enabled.) You can use this mode as a measure of prevention of wrong operation by children and restriction on operation by other than specified users.

SPLASH ID SCREEN
MAGE CAPTURE and SPLASH SCREEN in the menu become unavailable. SPLASH SCREEN will be set to ON automatically.

PAGE TOP PAGE TOP
Laser Pointer
A laser pointer is featured in the handheld remote control unit, allowing you to quickly and easily pinpoint or highlight specific parts of an image on screen.
PAGE TOP PAGE TOP
USB Terminal

A universal serial bus (USB) port is provided for connecting a USB mouse. This feature adds greater convenience and ease for projector operation.

PAGE TOP PAGE TOP
System Operation Remote

This unique remote controller allows the presenter to control operation of the projector and the DVD player and video cassette deck connected to it. Simply set the selection switch to the peripheral device being used (DVD or VIDEO).

PAGE TOP PAGE TOP
Multi-Language On-Screen Menu
This exceptionally convenient feature allows the user to choose the language used to display the on-screen operations menu. Some models allow you to choose from up to 10 (or 7) different languages, making Mitsubishi multimedia projectors ideal for international use.
PAGE TOP PAGE TOP
Disposable Filters

An easy-access air filter has been incorporated into the design to ease maintenance requirements. It is located on the bottom side of the projector in the back and can be removed for cleaning or replacement without requiring the projector to be unfastened from its brackets if mounted to the ceiling.

PAGE TOP PAGE TOP