|
|
 |
 |
 |
 |
Innovative technologies introduced to assist in providing presentations with greater impact, like multiple data ports for data input from various sources, a picture-in-picture feature that shows images from two different sources simultaneously and digital interfacing compatible with analog and digital signals.
|
 |
 |
 |
2-Live Picture-in-Picture |
 |
 |
|
2-Live Picture-in-Picture enables the presentation of images from two separate sources such as DVD and computer at the same time, effectively doubling visual information and presentation impact. Using this feature, you can present a smaller image inlaid in a corner of the main screen or spilt the main screen to show two images of equal szie. Either still or moving images, or a combination of both can be projected simultaneously. |
|
 |
Visual Information from Dual Sources
Information Expands Presentation Applications
|
 |
 |
 |
 |
 |
 |
 |
 |
| Real Motion |
| The 2 Live Picture-in-Picture feature has evolved to allow the projection of two moving/live images from different sources simultaneously. Of course, still images or a combination of still and moving images can be displayed as well. Data is processed at a fast 60 frames/sec, giving a smooth flow to moving images and making the projectors ideal for use in video conferencing. A zoom-in/out function is also included. |
|
 |
|
|
 |
 |
Digital-Expanded Zoom |
 |
 |
|
This feature allows you to choose a section of the main screen image and magnify it. As the data of the selected section is magnified via digital signal processing, details of the enlarged image remain true to the original. |
 |
 |
|
|
 |
|
|
 |
 |
Digital Interface |
 |
 |
|
The DVI terminal gives you easy connectivity to personal computers equipped with digital visual interfacing, and gives Mitsubishi Electric projectors full compatibility with analog signals and digital computers. |
 |
 |


 |
 |
|
|
 |
 |
Multiple Data Ports |
 |
 |
 |
Ports are provided for multiple data sources including computer, video and RS-232C serial port connections. |
 |
 |
 |
 |
 |
 |
 |
 |
 |
|
|
 |
 |
User Logo Display |
 |
 |
 |
Use every second possible to increase company name/logo recognition or present a specific image. Users can customize the projector to project a company and logo or any image of preference on the splash or mute screen. |
 |
 |
 |
 |
|
|
 |
 |
PC Card Slot |
 |
 |
 |
The ceiling-Use projector is equipped with a built-in anti-theft alarm. Once the projector is installed and the alarm is set, any unauthorized attempt to move the unit will cause the alarm to sound. |
 |
 |
 |
 |
|
|
 |
 |
V/H Keystone |
 |
 |
|
This projector automatically corrects vertical keystone distortion. For fine adjustment, press the KEYSTONE button on the projector or the remote control to display KEYSTONE, and adjust the image by pressing the , , , or button (or VOLUME + or - button on the remote control) |
|
 |
 |
 |
|
|
 |
 |
Vertical Keystone |
 |
 |
 |
This projector automatically corrects vertical keystone distortion. For fine adjustment, press the KEYSTONE button on the projector or the remote control to display KEYSTONE, and adjust the image by pressing the , , , or button (or VOLUME + or - button on the remote control) |
 |
 |
 |
 |
|
|
 |
|