|
Mitsubishi Electric has been strongly promoting
the information security business since 1996, the year MISTY1 was published.
In 2000, KASUMI, which is a variant of MISTY, was adopted as the mandatory
standard for the 3G mobile system W-CDMA. MISTY is now internationally
acknowledged as a strong and practical cipher. Also in 2000, Mitsubishi
Electric and NTT jointly designed the Camellia. Mitsubishi Electric is
currently offering these algorithms to various standardization bodies
such as the ISO, NESSIE and CRYPTREC for proposal. The Japan Ministry
of Public Management, Home Affairs, Posts and Telecommunications and the
Ministry of Economy, Trade and Industry have officially approved MISTY1
and Camellia for Japanese governmental use. It is most likely that the
NESSIE portfolio will be highly regarded as a vital component in the ISO
decision-making process while Mitsubishi Electric's encryption technology
becomes increasingly used on a worldwide scale.
Mitsubishi Electric's encryption technology development timeline:
| 1994 January |
Linear cryptanalysis is invented |
| 1994 August |
World's first experimental DES cryptanalysis |
| 1995 September |
MISTY published |
| 1995 November |
MISTY registered to ISO9979 |
| 1998 August |
Royalty free licensing of the MISTY patent |
| 2000 January |
KASUMI adopted as W-CDMA standard cipher |
| 2000 March |
Camellia (NTT and Mitsubishi Electric) published |
| 2001 May |
MISTY and KASUMI IP License |
| 2002 July |
KASUMI adopted in the GSM system |
| 2003 February |
MISTY1 and Camellia approved for use in Japanese
"e-government" |
| 2003 February |
MISTY1 and Camellia approved in the NESSIE project
|
MISTY
MISTY was developed
by Mitsubishi Electric in 1995 and is a family name of two encryption algorithms
MISTY1 and MISTY2, which has the world's highest-level of security and practicability.
MISTY1 and MISTY2 are both a 64-bit block cipher with a 128-bit key, which
can be used for data communication and electronic commerce in open networks.
The MISTY specifications have been published in full.
Camellia
Camellia is a next-generation 128-bit block encryption
algorithm jointly developed by Mitsubishi Electric and NTT, and supports
three key sizes: 128, 192 and 256 bits. The Camellia specifications have
been published in full. Camellia was designed not only for high security
levels suitable for the next generation but also for high performance in
any target platform such as embedded systems, where low power consumption
is mandatory and server computers, where utmost speed is a top priority.
About Mitsubishi
Electric
With over 80 years of experience in providing reliable, high-quality products
to both corporate clients and general consumers all over the world, Mitsubishi
Electric Corporation (TSE: 6503) is a recognized world leader in the manufacture,
marketing and sales of electrical and electronic equipment used in information
processing and communications, space development and satellite communications,
consumer electronics, industrial technology, energy, transportation and
building equipment. The company has operations in 35 countries and recorded
consolidated group sales of 3,649 billion yen (US$27.4 billion) in the year
ended March 31, 2002. For more information about Mitsubishi Electric, visit
Global.MitsubishiElectric.com
Inquiries (media only):
Public Relations Department
Tel: +81-3-3218-2346
|