| Background to the Joint
R&D "Secure and efficient implementation technology" is a vital R&D goal for achieving practical use. However, R&D has been faced with a trade-off between "security" and "efficiency". Therefore, Hitachi, Mitsubishi Electric and NTT launched the joint project and now they have succeeded in developing an implementation technology with the world's strongest security level while matching the efficiency of the existing products in the market. In March 2003, EU (European Union) approved NESSIE, a project to select the next-generation cryptographic algorithms. They selected "Camellia" jointly developed by Mitsubishi Electric and NTT, "MISTY1" by Mitsubishi Electric, and "PSEC-KEM" by NTT as recommended algorithms. Meanwhile, ISO (International Organization for Standardization) has been promoting the standardization of encryption goals by the Spring of 2004 at the earliest. In their deliberations, they have nominated not only "Camellia", "MISTY1" and "PSEC-KEM", but also "MULTI-S01" and "MUGI" by Hitachi, for international encryption standards. In addition, they have also been selected as recommended cryptographic algorithms by CRYPTREC: the cryptography evaluation project for e-governance by MPHPT (Ministry of Public Management, Home Affairs, Posts and Telecommunications) and METI (Ministry of Economy, Trade and Industry). Since the late 1990's, the U.S. and Japanese governments, EU and ISO, have actively promoted these encryption algorithm validation, selection, and standardization activities. They are now being almost completed, and the cryptographic algorithms that will be widely used in the first half of the 21st century are being listed up. The above Japanese cryptographic algorithm's excellent efficiency and their high commercial viability (LSI implementation) are highly regarded throughout these activities and it is likely that one or more of these Japanese company's algorithms will be widely used. Currently, ISO and CRYPTREC recognize that they need to emphasize "secure implementation", and they plan to establish the corresponding validation criteria and validation standards. As concern over "secure implementation of cryptosystems" increases, "CRESERC" is expected to be set into various application areas that require information security (for example, e-governance and ubiquitous communication systems) as the world's leading implementation technology in the field.
One of the important missions of NTT group is to contribute the achievement of a Ubiquitous Broadband society. NTT group concentrates on integrating the group on expanding Broadband Service on Photonic Access, Third Generation Cellular Phone, Wireless LAN, are provided for Access means, promoting the structure of distributing the contents of Movies and music, and enhance the providing contents. In November 2002, the Vision for a new optical generation is announced. For more information, please visit http://www.ntt.co.jp/index_e.html For media inquiries only: Hitachi, Ltd. Public Relations of Corporate Communications Division ; Konno Tel: +81-3-3258-2056 Email: atsushi_konno@hdq.hitachi.co.jp Mitsubishi Electric Corporation Public Relations Department Tel: +81-3-3218-2346 NTT Information Sharing Laboratory Group Planning Department, Public Relations Group; Iizuka, Sano, Chizuka Tel: +81-422-59-3663 Email: koho@mail.rdc.ntt.co.jp |