Space Systems Engineering Test
Engineering Test Satellites
Engineering test satellites test advanced technologies in orbit, which will be used to improve and enhance artificial satellites.
SERVIS
SERVIS
Verifies the performance of parts and equipment supplied by the private sector in space by applying to actual spacecraft for low-cost, short-cycle, high-quality (CFB) satellites. The development of SERVIS 1 and 2 will result in a low-cost commercial bus.
ETS-VIII
ETS-VIII
ETS-VIII is a geostationary satellite bus mounted with two of the world's largest antennas (19m x 17m), developed primarily to establish and verify technologies such as higher-traffic processing, mobile telecommunications, and high-accuracy satellite positioning, all of which are essential for space missions at the beginning of the 21st century.
USERS
USERS
USERS is an on-orbit experimental spacecraft system developed by USEF under a contract with METI and NEDO. It not only allows for long-term orbital experiments on a wide variety of challenges including the production of superconducting materials in the well-established enviroment, but also is capable of autonomously landing back on Earth.
TOP