Examples of Eco-Products and Hyper Eco-Products
Mitsubishi Electric manufactures products that give consideration to the environment in terms of Materials, Energy and Toxicity, or "MET." We have an internal certification program based on proprietary criteria that we use to designate products that help reduce environmental impact as "Eco-Products" and products with an even higher level of environmental performance as "Hyper Eco-Products." Here, we introduce some products that were certified in fiscal 2007.
Materials: Effective use of resources
Energy: Efficient use of energy
Toxicity: Avoidance of substances that are potentially harmful to the environment
Room Air Conditioner: MSZ-ZW407S
Technology to save energy based on usage conditions made possible by the evolution of Move-Eye
Factor rating of 2 or above
Use of plastic recycled in a closed-cycle
This air conditioner prioritizes both comfort and energy efficiency through the use of the "Human-Sensing Move-Eye," a feature that detects where people are located and automatically refines the area that receives air conditioning.

-
Closed-cycle recycled plastic from used home appliances is used in the indoor unit cross-flow fan and outdoor unit panel
Designed to be easy to clean during use and easy to disassemble when recycling
Existing pipes can be reused, which greatly reduces waste

-
The Move-Eye feature limits wasteful overcooling and overheating by controlling the perceived temperature; running the unit in automatic mode rather than continuous mode saves energy at a rate of 30%
"Human-Sensing Move-Eye" detects people and provides comfortable air conditioning to areas where people are located to improve energy efficiency by another 10%
The unit automatically cleans its own filter to prevent deterioration in energy efficiency caused by clogging, without any trouble to the user

-
Does not use any substances subject to the EU's RoHS Directive or Japanese Industrial Standards (JIS)'s J-Moss
Residential Heat Pump Water Heaters with Natural Refrigerant: SRT-HP37W1 (representative model)
(Factor calculated for SRT-HP46W1 model)
Received the Chairman's Award at the Energy Conversation Center, Japan's 2006 Energy Conservation Grand Prize Awards
Industry leading COP* (as of sales launch in June 2006)
*Coefficient of performance. A device's outputted energy divided by its inputted energy

This water heater uses a natural refrigerant that does not damage the ozone layer and features industry-class energy efficiency.

-
Fewer parts and greater use of plastic for a weight of 80 kilograms (16% reduction from the previous model)

-
Heat pump: High efficiency achieved with a newly developed twist-and-spiral gas cooler with a 4.9 COP rating (previous model was 4.5) and a CO2 compressor that uses Mitsubishi Electric's proprietarily developed joint wrap DC motor

-
Hot water tank: Insulating material is foamed polystyrene that does not include hazardous substances; Heat retention improved by 15%.
Package Air Conditioner (Wide Power Cassette Indoor Unit + Zupadan Slim Outdoor Unit): MPLZ-HRP BED Series
Strong market assessment as an air conditioner for truly cold climates
High energy efficiency and exceptional piping replacement technology for resource savings
Received Honorable Mention at the 2006 Electrical Manufacturers Awards sponsored by the Japan Electrical Manufacturers' Association

This heat pump air conditioner maintains its rated heating capacity even when the outdoor air temperature is -15C.

-
Existing piping and wiring can be reused, which substantially reduces waste
Plastic parts are labeled to make them easy to recycle

-
Uses the industry's first flash injection circuit* to improve heat capacity at low temperatures and improve energy efficiency by some 20%
Also, Move-Eye 360 prevents temperature irregularity and excessive cooling for additional energy savings of about 30%

-
Uses a refrigerant (HFC410A) with an ozone damage coefficient of zero
Does not use any substances subject to the EU's RoHS Directive or JIS's J-Moss
*A refrigerant circuit that limits rises in exhaust temperature when the outdoor air temperature is low, and maintains heating capacity with low outdoor air temperatures by compressing refrigerant when it is a two-phase mixture of gas and liquid
Inverter Compressor: PAC80 (for 8.0 kW inverters)
Received the Packaging Technology Logistics Award at the 2006 Japan Packaging Contest held by the Japan Packaging Institute
Helps improve the energy efficient performance of room air conditioners and package air conditioners
Factor rating of two or more

This compressor for inverters limits motor revolutions at an advanced level to help save energy.

-
Factor 2.02 achieved by 39% lower product weight than the previous model; the industry's lightest compressor for 8.0 kilowatt air conditioners
Export packaging uses molded paper products instead of conventional wood packaging

-
Low RPM performance improved through using Mitsubishi Electric's proprietary joint wrap DC motor and thermal caulking to fix the cylinders in place, which improves energy efficiency by 2% on an APF* basis
*Annual performance factor. Total amount of heat generated divided by the total amount of power consumed over that time.

-
Uses a refrigerant (HFC410A) with an ozone damage coefficient of zero
Does not use any substances subject to the EU's RoHS Directive or JIS's J-Moss
Inverter: FREQROL-F700
- Received Honorable award at the 2006 Electrical Manufacturers Awards sponsored by the Japan Electrical Manufacturers' Association

Using an inverter for fan or pump application is more efficient and saves more energy than conventional flow rate control using a damper, valve, or motor on-off control.

-
Designed to extend the life span of major consumables, such as capacitors and cooling fans, the design life is ten years to effectively help save resources.

-
By using an inverter for fan or pump application and controlling the flow rate by changing the motor speed, it achieves a higher level of energy saving compared to the flow rate control using a damper, valve, or motor on-off control. Optimal excitation control (a distinct function in FREQROL-F700) makes more energy saving possible compared to conventional V/f control.

-
Complies with the EU RoHS Directive to use alternatives to all six hazardous substances
Wire-Electrical Discharge Machine: FA20PS Advance
Won the Innovation Prize at the 2006 Japan Invention and Innovation Awards sponsored by the Japan Institute of Invention and Innovation

This wire-electrical discharge machine is a machine tool that utilizes the discharge phenomenon to precision-process metals using electrode wire that is the size of a strand of hair.

-
Preventing wire electrode breaks improves processing yields and reduces wire electrode waste

-
Eliminating wire electrode breaks and controlling energy to match processing variation cuts processing time in half (doubling energy efficiency)

-
Uses screws and steel sheeting with hexavalent chromium-free coating; CFC substitute used to cool the processing fluid