Transmitting real-time images of disaster areas.
Supporting rapid and accurate disaster prevention measures.
Overview
Systems that can transmit high-altitude, real-time disaster area image information via a geosynchronous orbit satellite to relevant emergency organizations when disasters occur are under consideration. Mitsubishi Electric is developing an active phased array antenna*1 for use in helicopter on-board satellite communication, and has supplied some to NICT*2. This cutting-edge antenna and the high-frequency circuit technology used make the equipment smaller and thinner than conventional systems.
Technology Point
Using this active phased array antenna technology enables instantaneous and non-stop electronic communication with satellites, even when the helicopter's position changes.
In addition to small, lightweight antenna components*3, which can be easily mass produced, we are developing high-frequency circuits that have the world's highest-density wiring.
We will improve the antenna gain by developing novel antenna element arrangement and ensure high-quality moving image transmission with reducing interference to the other satellites.
- Notes
- *1: The flat antenna can control the radiation beam direction electronically without use of a mechanical driver.
- *2: National Institute of Information and Communications Technology (NICT)
- *3: Small antenna consisting of an active phased array antenna. Multiple antenna components are arranged systematically