MISTY Decipher and win contest!
<< back to gate
1903
Sherlock Holmes Cipher
Entrance STAGE 1 STAGE 2 STAGE 3 STAGE 4 STAGE 5
About MISTY
STAGE3
1903
Sherlock Holmes Cipher
Sir Arthur Conan Doyle often introduced encryptions in his popular Sherlock Holmes series. In "The Dancing Men", Holmes succeeds in deciphering a message that encrypts alphabets into dancing men.
* Dolls holding flags indicate breaks between words.
image
* Mitsubishi Electric has created a graphic representation of the "Dancing Men" with reference to the original. Please note that there may be slight differences.
* The "Dancing Men" in the encryption quiz below have been created as an original by Mitsubishi Electric and do not appear in the novel.
       
  Decipher the code!
Although there are "Dancing Men" that do not appear in the list above, read Holmes' clue to decipher and put the answer in the box.
{Sent message} PLVWB
Verify  
  Write down the deciphered word (6 letters) and click the "Verify" button to proceed.      
       
pagetop