News Releases
 

Media Contacts:

Mitsubishi Electric Corp.
Public Relations; Mr./Ms. Morii; Tel.: +81-3-3218-2172

IBM Japan, Ltd.
Public Relations; Mr./Ms. Takahashi; Tel.: +81-3-5563-4304

 
 

Mitsubishi Electric and IBM Jointly Develop Integrated LSI Optimized for HDD Control

Tokyo March 4, 1997 -- Mitsubishi Electric Corp. (president: Takashi Kitaoka) and IBM Corporation (chairman: Louis V. Gerstner) have jointly developed an integrated LSI that incorporates a microcomputer, a hard disk controller (HDC), and flash memory in a single chip to be installed on IBM Corp.'s hard disk drives (HDDs).

The LSI is to be manufactured by both IBM Corp. and Mitsubishi Electric and will be installed on HDDs manufactured by IBM Corp., beginning in September 1997.


The Merits of Integration
  1. Twice the Performance
    By optimizing microcomputer CPUs for HDD control and incorporating them in a single chip, the speed of data transmission between the CPU, HDC, and flash memory increases, resulting in twice the performance.

  2. Power Consumption Reduced by 30%
    Power consumption is reduced by 30% by decreasing the total number of pins and making processes more detailed.

  3. Mounting Area Cut in Half
    By integrating an 80-pin microcomputer and a 128-pin HDC into a 144-pin package, the mounting area is reduced by one half.

  4. Cost Reduction
    By integrating the components into a single chip, the costs of the chip and the package are reduced significantly.

    Furthermore, once the LSI enters volume production, costs will be reduced even further by converting the flash memory into mask ROM.


Product Features
  1. A CPU Core Optimized for HDD Control
    The instruction set has been optimized for disk application and the code has been reduced by 30% from past codes.

    Also, in addition to strengthening the hardware, the speed of data transmission between the flash memory and the HDC has been increased, doubling the data processing capabilities.

  2. Debugging Environment Adapted to an Integrated LSI
    A debugging circuit with break, trace, and download functions is incorporated in the integrated LSI, creating an environment for program development and debugging that uses the internal flash memory. As a result, there is no need to output the microcomputer bus externally, making it possible to limit the number of pins to 144. This contributed greatly to decreased power consumption, mounting area, and costs.

    Furthermore, program development and debugging can be performed with the integrated LSI installed on the circuit board, exactly the same environment as in actual use, allowing for high-quality debugging.


Background to Development

    In the past, IBM Corp. HDDs included Mitsubishi Electric's microcomputers with internal flash memory and IBM Corp.'s HDCs.

    In accordance with the increasing capacity and performance of HDDs, microcomputer and HDC performance has been improved, but to respond to further increases in capacity and performance in the future and to implement significant reductions in cost, IBM Corp. and Mitsubishi Electric jointly developed an integrated LSI that incorporates a microcomputer and HDC.

    The integrated LSI will initially be installed on HDDs shipped in September 1997, and IBM Corp. plans to expand it to all IBM HDDs developed in Japan.


Product Specifications
  1. Performance Details

    Microcomputer:
    Mitsubishi original 16-bit CPU core
    Interrupt controller; A/D converter; serial I/O; multifunction timer
    Debugging circuit
    RAM of 2K bytes

    Flash memory: 48K bytes

    HDC:
    IDE controller with ULTRA DMA (35Mb/e)
    16-bit EDO DRAM controller
    NO-ID (TM) disk controller circuit
    High-performance error correction circuit

  2. Operating speed: 40MHz

  3. Package: 144-pin QFP

    Future Developments

    To support low costs, IBM Corp. and Mitsubishi Electric will develop even higher performance integrated LSI products and incorporate them into their products.

    Also, the companies are considering further integration including internal DRAM.

  Return to same year archive