News Releases
 
  NO.0447
 

Mitsubishi Electric Develops 105MB Flash ATA PC Card


22.5MB CompactFlashTM Card Largest Capacity in Industry, Based on 64M-bit AND-type Flash Memory Chips



Mitsubishi Electric Corporation (President: Takashi Kitaoka) announced today that the company has developed a new 105MB flash ATA PC card, the largest capacity Type-1 PC card (3.3 mm thick) currently available on the market. This PC card is based on the new 64M-bit, AND-type flash memory chip designed jointly by Mitsubishi Electric and Hitachi Corporation specifically for large-capacity storage devices. Mitsubishi Electric has also developed a 22.5MB CompactFlashTM memory card equipped with the same flash memory chip. The company will begin shipment of samples of the new products on September 22, 1997.

"These two new products clearly highlight the small size, low power, and high capacity advantages of Mitsubishi Electric's approach of placing all the controllers on a single chip," said Dr. Koichi Nagasawa, director and deputy general manager of Mitsubishi Electric's Semiconductor Group. Mitsubishi Electric is focused on the promising market for notebook computers, digital still cameras, and other portable electronic devices which require large memory capacities in very small spaces," continued Dr. Nagasawa. "These two new additions to our PC card line demonstrate our firm commitment to this market and also place us in a strong position vis-a-vis our competitors."

Product Outline

Both new industry-standard products are PC cards developed in full compliance with PC Card ATA and the CompactFlashTM Specifications Rev. 1.1 published by the CompactFlashTM Association (CFA), a standardization organization for CompactFlashTM memory cards. By installing standard card device drivers which come with notebook computers equipped with PC card slots, users can read and write data freely using PC flash memory cards. Moreover, the new PC cards support the IDE interface and can be directly connected to fixed hard disk drives in personal computers. They can operate at as low as 3.3V, and are ideal for digital still cameras and small portable data terminals whose markets will continue to grow. Monthly production is expected to reach 10,000 units at year-end.

Product Features

1. Thin profile and largest capacity in industry.

Mitsubishi Electric has adopted a new single chip controller circuit, instead of a conventional three-chip configuration. The new 105MB flash ATA PC card and the 22.5MB CompactFlashTM card come equipped with the 64M-bit AND-type flash memory chip optimized for large-capacity storage devices and a proprietary single-chip controller LSI specially designed for the new products.

2. 5V/3.3V dual voltage operation

3. Low power consumption

30mA/write mode and 25mA/read mode (at 5V operation)

4. High reliability with built-in error correction

An error correction circuit is built into the new single-chip controller LSI for higher reliability during data transfer.

5. High-level interface compatibility

CompactFlashTM cards may be used as ordinary ATA PC cards using adapters available from commercial venders. This convenient feature makes it easy to download data stored in CompactFlashTMcards to notebook computers and other general-purpose peripherals equipped with PC card slots for further data processing and editing.

Product Background

Notebook computers, sub-notebook computers, PDAs, hand-held personal computers, digital still cameras, and other small-sized electronic equipment have been gaining popularity in recent years. Consequently, flash-memory-based PC cards have attracted a great deal of attention as low-cost, large-capacity memory devices for data exchange. Notably, flash ATA PC cards and CompactFlashTMcards are considered particularly versatile types of external memory media because they can perform read and write operations with data transfer protocols comparable to those of ordinary hard disk drives. Mitsubishi has already commercialized 5-mm-thick flash ATA PC cards (Type-2 PC card) with a storage capacity of 15MB-75MB as well as 2.8MB/6.2MB CompactFlashTM cards. In response to increasing demand for larger capacity and thinner flash memory cards, Mitsubishi Electric has newly developed 3-mm-thick flash ATA PC cards (105, 90, 75, 60, 45, 30, 15, 15, 7.5MB) and CompactFlashTM cards (22.5, 15, 7.5MB).

Sample Prices and Storage Capacity

Model

Storage Capacity

Unit Price

Scheduled Sample Shipment Date

MF0105M-03ATXX

105MB

\223,000

October 20, 1997

MF0090M-03ATXX

90MB

\193,000

September 22, 1997

MF0075M-03ATXX

75MB

\163,000

September 22, 1997

MF0060M-03ATXX

60MB

\133,000

September 22, 1997

MF0045M-03ATXX

45MB

\103,000

September 22, 1997

MF0030M-03ATXX

30MB

\ 73,000

September 22, 1997

MF0015M-03ATXX

15MB

\ 43,000

September 22, 1997

MF007M5-03ATXX

7.5MB

\ 28,000

September 22, 1997

Model

Storage Capacity

Unit Price

Scheduled Sample Shipment Date

MF022M5-03AAXX

22.5MB

\ 55,000

October 20, 1997

MF0015M-03AAXX

15MB

\40,000

September 22, 1997

MF007M5-03AAXX

7.5MB

\ 25,000

September 22, 1997

Key Product Specifications

1. External Size

Flash ATA PC card: 54.0 (W) X 85.6 (L) X 3.3 (T) (mm)

CompactFlashTM card: 42.8 (W) X 36.4 (L) X 3.3 (T) (mm)

2. Power Requirement: 5V +/-10% or 3.3V +/-5% (single power source operation)

3. Read/Write Rate: 300KB/sec (typical)

4. Host Transfer Rate: 8MB/sec

CompactFlashTM is a trademark of SanDisk Corp. (U. S. A.).

  Return to same year archive