Mitsubishi Electric
Commences Sales of the 7900 Series, the Top-Line
Series of the World's No.1 16-bit Microcomputer
7700 Family
Tokyo, October 1, 1997 -- Mitsubishi Electric Corporation (president:
Takashi Kitaoka) hereby announce the development of the 7900 series,
which incorporates increased CPU processing power, as a top-line
member of the 16-bit microcomputer 7700 family used to control the
hard disk drives for computers and other computer-related equipment,
such as office appliances and portable information equipment. The
shipment of samples for the six available models, which include
built-in flash memory capable of operating on a single power supply,
will commence on October 6, 1997.
Development History
Our 16-bit microcomputer 7700 family
is widely used throughout the manufacturing industry as system
controllers for hard disk drives, CD-ROM units, printers, PPCs,
mobile telephones, personal handy-phones and other related equipment,
and there is an increasing demand for high levels of data processing
capabilities to cope with the increases in functionality and performance
in such equipment. There is also a demand for microcomputers
equipped with flash memories that are able to cope easily with
program bugs, modifications to specifications and software up-grades
inherent with the advent of large-scale programs and wide-ranging
diversity in application equipment.
Demand for products that provide
high-speed operations on low voltage power for energy-saving purposes
is also prevalent.
In order to provide solutions to
these demands, Mitsubishi Electric developed the 7900 series as
a top-line member of the 7700 family.
Product Features
(1) A three-fold increase in CPU
performance and 30% improved program code efficiency over the
7700 series
- The number of commands have been
expanded to 203 while maintaining upward compatibility with the
basic 7700 CPU commands (103 commands) to provide efficient command
setting.
- The fastest command is executed
within the space of one cycle, and this is reduced to 50ns when
connected to an external clock input with a 20MHz frequency level.
- The chip employs a method of separating
the code path and data path, and this, in combination with a 10-byte
command queue buffer and a 4-byte data buffer in the path interface
unit, enables high-speed data processing.
(2) Built-in flash memory that operates
on a single power supply of 5V/3.3V to enable block erasure
[20MHz operation possible with 3.3V
(the industry's fastest)]
- 5V/3.3V operation on a single power
supply made possible by 0.5µm DINOR flash memory process
technology.
- As writing and erasure is possible
with a single power supply, overwriting can be easily performed
on-board.
- Block erasure and CPU overwriting
is also supported.
(3) Development environments which
use on-chip debugging functions supported
- The break functions and trace functions
that used to be performed with external emulators have been built
into the chips, enabling the debugging of microcomputers that
operate at high speeds with low-cost emulators.
(4) Low power consumption
- Developed with the energy-saving
power capabilities of the reputable 7700 family.
(5) Reduction of unwanted radiation
and improved noise resistance
- Unnecessary signal fluctuations
restrained.
- Drive performance optimized.
- Noise canceler improved.
Product Specifications
(1) Built-in high-performance 7900
CPU
- 203 basic commands.
- 50ns execution time for the fastest
command (when connected to an external clock with an input frequency
of 20MHz)
(2) Wide range of memory types
- External memory type: Built-in
2K RAM
- Flash memory: Built-in 256 kilobyte
flash memory, built-in 6 kilobyte RAM
- Flash memory: Built-in 128 kilobyte
flash memory, built-in 4 kilobyte RAM
(3) Powerful peripheral functions
- DMAC 4ch
- DRAMC (supports Fast Page/EDO)
- Eight 16-bit timers, two serial
I/O channels
- Four 10-bit A-D converter channels
(4) On-chip debugging function
Product descriptions
Three types of the 7900 series will
be marketed during the first phase; the external memory type,
the built-in 256 kilobyte flash memory type and the built-in 128
kilobyte flash memory type. Each of these will be available in
the 5V power voltage model and the 3.3V power voltage model, making
a total of six different models.
| | Model name
| Power voltage
| Operating frequency for external clocks
| Date of sample shipping
| Sample price
|
| External Memory type
| M37920S4CGP
| 5.0V |
20MHz | October 6, 1997
| 1,000 yen
|
| | M37920S4MHP
| 3.3V |
12MHz | October 6, 1997
| 1,000 yen
|
| 256 kilobyte flash memory type
| M37920FGCGP
| Single power supply of 5.0V
| 20MHz |
November 1997
| 2,500 yen
|
| | M37920FGMHP
| Single power supply of 3.3V
| 20MHz |
November 1997
| 2,500 yen
|
| 128 kilobyte flash memory type
| M37920FCCGP
| Single power supply of 5.0V
| 20MHz |
November 1997
| 2,000 yen
|
| | M37920FCMHP
| Single power supply of 3.3V
| 20MHz |
November 1997
| 2,000 yen
|
Future development
5V built-in flash memory model
Mask ROM model
5V models 256
kilobytes 256 kilobytes
M37920FGCGP
M37920S4CGP 128
kilobytes 128 kilobytes
M37920FCCGP
3.3V built-in flash memory model
Mask ROM model (3.3V)
3.3V models 256
kilobytes 256 kilobytes
M37920FGMHP
M37920S4MHP 128
kilobytes 128 kilobytes
M37920FCMHP
Production schedule
End of 1997: 100,000/month
Spring 1998: 500,000/month
- ### -
|