Mitsubishi Electric Develops Lifestyle-Based Disease Monitoring Network System
Mitsubishi Electric Corporation has
developed a lifestyle-based disease monitoring network system
that will serve to expand the company's business in the home health
care market.
As a health promotion measure for
our aging society, this system will become an important factor
in preventing and suppressing the progress of lifestyle-based
diseases. The system was developed in cooperation with Nihon
Colin Co., Ltd. (Masatoshi Shinoda, president).
The new system comprises a sensor
that accurately measures blood pressure on a daily basis. A communications
network (LAN, ISDN, PHS) and data servers, then enables diagnosticians,
company physicians and health care personnel to monitor trends
in blood pressure fluctuation. This in turn will prevent diseases
caused by hypertension of which the patient is normally unaware,
such as heart disease, cerebro-vascular disease and renal disease.
It is also expected to be effective in reducing health insurance
costs and health care costs by contributing to the prevention
of the sudden death of hard-working company personnel and by aiding
daily health management.
Main Features
This newly developed system allows
the use of magnetic cards to store and input data on individuals.
It is also equipped with a reasoning system that records the
blood pressure data of each individual, analyzes the trend of
blood pressure fluctuations based on the data stored on the cards
and selects comments according to the characteristics of the data.
Several hundred of these comments have been prepared. Thus,
when the blood pressure of an individual is measured, a comment
such as "Your blood pressure is high compared with the average
blood pressure of people your age, so be careful concerning daily
activities, exercise and eating," will be printed out, together
with the measured data. This system provides the following benefits:
1. Increases the awareness of individuals concerning health management.
2. Enables detailed comments tailored
to individuals whose blood pressure is becoming high.
3. Helps people develop the habit
of being more aware of their own serious illnesses and of sudden
changes in their physical conditions.
4. Enables individual consultations
concerning lifestyle-based diseases even in remote areas by using
intranets or the Internet. For example, blood pressure can be
measured at home or on the job and comments can be received immediately
from the family or company physician.
5. As the comments can be changed
from the center, comments and advice may easily be adapted to
the particular characteristics of the data transmitted from each
place of operation.
Future Development
1. The new system is slated to be distributed to businesses, health
insurance unions and local government bodies.
2. In the future, a comprehensive
health management system will be realized by linking the long-term
accumulation of data on illnesses with diagnostic data.
3. A remote medical system including
home medical terminals is also envisioned for the future.
Development Background
The average age of the business population
of Japan is gradually creeping upward each year. At the same
time, the nature of work is changing from labor-intensive to intellectual
production. In addition, stress levels seem to be increasing
and there have been many recent cases of sudden deaths within
companies. Lifestyle-based diseases, which first become noticeable
when people are in their thirties, are quietly advanced due to
excesses at work. Lifestyle-based diseases suddenly appear as
the second most serious problems in medical expenses for those
in their forties, while they are by far the highest for those
in their fifties and over.
In Japan, one person in six has high
blood pressure, which is the cause of lifestyle-based diseases,
and the percentage of people with this condition is expected to
continue to grow in the future. Most people with the condition
are not aware that they have high blood pressure, which is feared
as a silent killer, and hypertension is also an important risk
factor in cerebro-vascular disease, heart disease and renal disease.
If hypertension is left untreated, the probability that it will
contribute to the development of one or more of these diseases
gradually increases. The condition also leads to hardening of
the arteries and in some cases may result in sudden death.
Countermeasures against lifestyle-based
diseases are extremely important from the viewpoint of promoting
public health and reducing health care costs.
For businesses as well, working to
prevent the contraction of diseases and sudden deaths among hard-working
employees is expected to play a role in enhancing the soundness
of national health protection. The first step in the prevention
of high blood pressure is to develop the habit of correctly measuring
one's own blood pressure on a daily basis and of being aware of
the trend of one's blood pressure fluctuations.
System Configuration
- Automatic oscillometric-type sphygmomanometer
- Magnetic card system (no. of persons
registered: 80/unit; JIS Type 2)
- Windows NT compatible server/client
system
Development Details
This system was developed by changing
to a device that can chart the height, weight and blood pressure
of an individual as a time series, combining this information
with data on the lifestyles of individuals (consumption of alcoholic
beverages, smoking, date of birth, etc., are recorded on magnetic
cards), incorporating a device to estimate the blood pressure
symptoms of subjects, developing a sphygmomanometer that issues
comments aimed at the prevention of high blood pressure, adding
servers for the long-term storage of individuals' data and management
of individuals' health, adding client terminals that provide users
with comments from company physicians, nurses, nutritionists,
and other health care personnel, and adding communications devices
to connect all of the other components of the system into a single
network.
###
|