News Releases
 
[News release domestically issued on December 15, 1997]
NO.0467
 

For Making the Compact Sized and Light Weighed Converter for Railway Propulsion into Reality, 2.5kV/3.3kV HVIGBT Modules for the Second Generation Is Now Available on the Market




Mitsubishi Electric Corporation has developed a second generation of 2.5 kV/3.3 kV HVIGBT* Modules for high power industries such as electric traction companies, power plants, and production plants. The sample shipments will start as of January, 1998.

With these models, reductions in the heat emission from the built-in power semiconductor chip (to the lowest level in the industry) as well as improvements in the heat conductivity (to the highest level in the industry), have allowed the number of cooling fins necessary for radiating heat during current carrying to be reduced and a substantial reduction of power loss can now be achieved, thereby achieving a compactness in terms of volume, as well as weight, and simplification of heat design realized for the railway propulsion and steel rolling, etc.

* HVIGBT: High Voltage Insulated Gate Bipolar Transistor

  Return to same year archive