| |
Mitsubishi Electric Launches the FPR-MK
II Series of Fingerprint Checkers
Tokyo, February 10, 1998 -- Mitsubishi Electric Corporation
(president: Takashi Kitaoka), through Mitsubishi Corporation (Hong
Kong) Limited, has received an order from the Government of the
Hong Kong Special Administrative Region (IIKSAR) to design, manufacture,
supply, deliver, install, test, and commission an S-band Klystron
Doppler Weather Radar System for the Hong Kong Observatory (HKO).
This order is a replacement of one of the two radars which HKO
currently
operates.
This order represents Mitsubishi Electric's third project involving
S-band Doppler Weather Radar in the Asian market following the Singapore
Changi Airport project and the Kuala Lumpur International Airport
project.
The state-of-the-art radar system for the HKO, which is scheduled
to be commissioned in January 1999, will have the following features:
- Equipped with the latest developed digital receiver, a highly
stable klyston-type transmitter and a large 8.5-metre antenna,
the system will be capable of real-time detection and tracking
of areas of precipitation, thunderstorms, tropical cyclones and
other weather phenomena. Rainfall intensity can be determined
accurately within a radius of at least 500 kilometers and wind
velocity within at least 250 kilometers.
- The radar station will be unmanned and the system will be highly
automatic, capable of being controlled and monitored remotely
at the HKO Headquarters.
- Dual-Doppler processing for deriving real-time horizontal winds
is the first in the world in terms of operational weather forecasting
as well as numerical weather prediction.
- 3-dimensional display of radar images in animation, a new and
innovative method for analysts of radar data, will also be a key
feature of the system.
The System will provide real-time information for tracking and
estimating the intensity of tropical cyclones. The 3-dimensional
display of tropical cyclone information will be the world's first
operational system with such capabilities. It will open up a new
era in the observation of tropical cyclones by radars. This new
system will enhance the accuracy of tropical cyclone forecasts and
warnings.
The equipment of the System will be located at three (3) sites,
namely, the Radar Station at Tai Mo Shan around 950 meters above
sea level, the HKO Headquarters and the Airport Meteorological Office
at the new airport at Chek Lap Kok.
- ### -
|