Mitsubishi Electric Receives Order for
Weather Radar System for the Hong Kong Observatory
Even easier to use, one-fifth the size of previous
models,
and one-third the price.
Tokyo, March 2, 1998 - This year, on April 1st, Mitsubishi
Electric Corporation (President: Takashi Kitaoka) will launch its
FPR-MKII Series of fingerprint-checking devices. Since every human
fingerprint is unique to its owner, and remains unchanged for life,
fingerprint checkers are able to uniquely and reliably distinguish
individuals by their fingerprints. This means that access to site
entrances, safes, computers and the like, traditionally controlled
using keys, can now be controlled using fingerprint checkers.
The new fingerprint checkers will also be exhibited at the '98
SECURITY SHOW (to be held at Tokyo Big Sight) from March 3.
Launch outline (typical model)
|
Product name, model name
|
Specifications
|
Price
|
Mitsubishi Fingerprint Checker,
FPR-DT MK II
(designed for connection to personal computers) |
Checking method: "No-PIN" fingerprint
identification (subject simply places finger on device) Maximum
number of registered fingerprints: 100 Reading and identification
time: 1 second on average
Error rate:
False positive: 0.1% or less
False negative: 0.3% or less
Size: 41mm (width) 53mm (height) 90mm (depth)
|
98,000 yen |
* Excluding tax
In addition to the personal-computer model described
above, Mitsubishi Electric will be releasing other models for entrance/exit
control and time and attendance systems. The FPR-MK II Series will
comprise six models in all, and Mitsubishi Electric plans to ship
some 10,000 units (for the series as a whole) in the first fiscal
year.
Outline of products
Drawing on experience gained through impressive
sales of its earlier fingerprint checker, launched in January 1996,
the company has produced a single module combining all the functions
required for fingerprint identification, including the processing
involved in sensing and checking fingerprints, and storage of fingerprint
data. By improving the fingerprint sensor and fitting the processing
circuitry onto a single chip, Mitsubishi Electric has arrived at
a product only one-fifth the size of its predecessor at only one-third
the price. Thanks to a highly-reliable pattern-matching algorithm
improving on the basic features of the earlier model, the new products
can perform no-PIN fingerprint identification, requiring the subject
merely to place his or her finger on the device. This has made them
even easier to use than before.
Special features of products
(1) Much easier to use: the subject is not required
to enter a personal ID number, but simply places his or her finger
on the device, and identification is then carried out in a mere
second.
(2) The new models cost only one-third the price
of their predecessor, and are only one-fifth the size.
(3) The comprehensive product line-up covers a
wide range of applications, including models designed for connection
to a personal computer, entrance/exit control and time and attendance
systems.
FPR-MK II Series: Details of Special Features
1. Fingerprint identification in just one second
Mitsubishi Electric's latest range of fingerprint
readers comes with a new standard feature: all the subject has to
do is place his or her finger on the reader, without typing in an
ID number at all. Using a highly-reliable pattern-matching algorithm,
one individual's fingerprint can be identified from a large number
of registered prints (up to 100) in merely a second, with an error
rate (for false positives) of less than 0.1%, or in other words,
less than one error for every thousand readings.
2. Compact size and low price
By improving its proprietary super-compact fingerprint
sensor, and fitting the processing circuit -- containing the new
algorithm -- on to a single chip, Mitsubishi Electric has managed
to bring the price down to one-third that of its predecessor (the
FPR-DT).
The new super-compact fingerprint-matching module
contains the fingerprint sensor and all the functions needed for
fingerprint identification, such as match-processing and fingerprint
data memory. This has made it possible to reduce the size of the
whole unit to one-fifth that of the previous model (the FPR-DT).
3. Comprehensive product line-up
Mitsubishi Electric has expanded its product line-up
by offering a group of products covering a wide range of applications:
there are models designed to be connected to a personal computer,
models for use in controlling the entrance/exit of personnel, tracking
staff time and attendance, and so on.
1) The FPR-DT MKII is designed to be connected
to a personal computer, and can identify individuals by fingerprint,
for the purpose of controlling access to computers, networks and
so on.
2) The FPR-200AD MKII, the FPR-1000AD MKII and
the FPR-1000CS MKII are designed for entrance/exit control, using
fingerprint identification to ensure that only authorized personnel
pass in or out of the doorway in question.
3) The FPR-200 HG MKII and FPR-1000 FG MKII are
designed for time logging and attendance systems, using fingerprint
identification to check employees' working hours.
Typical applications and prospects
Thanks to the reduced price of the new products,
Mitsubishi Electric envisages that the FPR-MK II Series will come
increasingly into demand as operation/input devices for established
applications such as entrance/exit control and time and attendance
systems.
The increasing popularity of the Internet, electronic
commerce and on-line information services is creating a need for
security technologies to protect users against high-tech fraud.
These handy, user-friendly fingerprint-checking devices capable
of restricting access to authorized personnel, are likely to be
used as an optimal, reliable means of identifying individuals.
Thanks to the new, compact, low-cost fingerprint-matching
module, the products in this series can be combined with appliances
and devices traditionally controlled using keys: for example, they
can be used for rooms/apartments, safes, lockers, cars and so on.
The new products are slated for active marketing
overseas as well as in Japan.
- ### -
|