Mitsubishi Electric
Develops StrengthErgo Therapeutic Exercise System to Prevent Patients
Becoming Completely BedriddenS
-- Helps to restore physical
functionality as part of rehabilitation for all levels of disability
--
Tokyo, June 2, 1998 -- Mitsubishi Electric Corporation (President:
Takashi Kitaoka) has developed an exercise system called StrengthErgo.
The object of the system is to help rehabilitate patients by restoring
effective physical functionality.
Up to now, the absence of an exercise
system versatile enough to cater for all levels of disability
has prevented partially paralyzed patients from undergoing the
sort of positive rehabilitation that would give them the day-to-day
independence they need. Patients in need of urgent rehabilitation
have been similarly deprived. The new system provides patients
of every sort with the opportunity to follow a training program
tailored specifically to their needs while at the same time enjoying
a video.
During the development of the system,
Mitsubishi Electric was provided with clinical advice by Dr.
Sumio Yamada, Clerk Examiner of the Department of Rehabilitation
Medicine at St. Marianna University School of Medicine in the
city of Kawasaki in Kanagawa, Japan.
Development objectives
The progressive aging of Japan's
population is making it increasingly important to find ways of
helping old people to regain their strength and of preventing
them from becoming bedridden. To enhance the quality of old people's
lives by enabling them to remain independent on a day-to-day basis,
the Public Nursing Care Insurance System, which is due to be introduced
in the near future, will be called on to cater not only for the
provision of straightforward nursing care but also for the establishment
of active rehabilitation programs.
Rehabilitation programs currently
tend to focus on training disabled persons to get around, using
various means of transport, getting in and out of the bath, and
so on. However, they still have a long way to go in helping people
to restore and/or maintain their independence through programs
of exercise designed to rebuild muscular and overall physical
strength. This is because, among other things, most exercise
equipment used for rehabilitation purposes is of a sort designed
to enable able-bodied persons to enhance their fitness by improving
their heart and lung functions rather than to help patients who
have suffered partial paralysis as the result of a stroke -- a
problem very much on the increase today -- to recover their physical
strength.
Mitsubishi Electric undertook the
current development program in response to the growing need for
exercise equipment for persons undergoing courses of rehabilitation.
Features of the StrengthErgo
therapeutic exercise system
1. Training for people with
every kind of physical impairment
The system can be used to rehabilitate
any patient with functional impairment of his/her legs due, for
example, to the partial paralysis that is one of the common after-effects
of a stroke. Cycling exercises are used to simultaneously measure
patients' left and right leg strength, thereby enabling continuous
monitoring of the efficacy of their training. It is thus a simple
task to adjust training programs to meet the precise needs of
individual patients.
2. Fast rehabilitation achievable
by adjustment of the exercise position
The exercise position of the equipment
can be adjusted to accommodate patients in various postures from
lying face up to occupying a regular sitting position.
3. Training combined with
the enjoyment of a video
To promote the continuity that constitutes
such an important element of any exercise program, StrengthErgo
also includes an enjoyable cycling video as an integral part of
the program. Video images of street scenes, mountain scenery,
the changing seasons, new discoveries and so on help the patient
to achieve the sort of inner fulfillment that can help them relax
and enjoy their exercise program.
The System
I Exercise functions
to suit specific disabilities
1) Individual left and right
drives
Conventional exercise bicycles are
fitted with a single crankshaft. This is not suitable for patients
whose disability is such that the strength in their left and right
legs is not uniform. The present system provides for the pedal
crankshaft to respond independently to differences in the force
applied by left and right legs. This enables left and right legs
each to be exercised at a pace which suits them and enables separate
load values to be set for left and right pedals to match the patient's
needs.
2) Assisted drives
In addition to the drive load device,
each pedal is also fitted with an assist motor to enable the pedals
to be switched into a mechanical drive mode. The motor is used
to drive the pedals mechanically to help rehabilitate patients
who are paralyzed down one side only, for example, or patients
with damage to their spinal cord, who may find it difficult to
pedal at all. The assist motor function can also be set such
that it is activated to help the patient continue pedaling if
he/she tires and allows his/her pedaling rate to drop below a
specified level.
3) Measurement of leg strength
The system measures muscle strength
in situations in which the muscles are actually being used. By
putting the equipment into isokinetic mode -- an exercise situation
in which the speed is held constant -- leg strength can be evaluated
by measuring the load torque applied when the patient presses
down on the pedal.
4) Setting the exercise program
By combining the independent left
and right drive function and the assisted drive function, the
exercise load can be freely and easily set to provide a therapeutic
exercise program tailored to the needs of the individual patient.
The program can be modified during training to accommodate changes
in the patient's condition.
II Adjusting the exercise
position
A reclining seat and a pedal height
adjustment mechanism enable the exercise bicycle to be set to
a position that best suits the patient. As the exercise position
of the equipment can be adjusted to accommodate patients in various
postures from lying face up to occupying a regular sitting position,
it can be used to start rehabilitating patients from the moment
they are able to get up out of bed. A revolving saddle also makes
it easier for patients to get on and off.
III Cycling video software
The exercise system is also provided
with video software to help patients derive greater enjoyment
from their exercise sessions. Images of street scenes, mountain
scenery, the changing seasons and so on are used to help the patient
achieve the sort of inner relaxation that will enable them to
enjoy their exercise program. The software also enables the pace
and quantity of exercise to be matched with cycling speed, gradient
and distance. Patients can use these functions to adjust the
pace of their exercise program to suit their physical strength.
This makes it possible for them to enjoy the satisfaction of
achieving their chosen goal.
By increasing the patient's interest
in their health, the system also opens the way to enjoyable daily
training sessions for the prevention of obesity, for example.
Possible clinical uses
(1) For patients with impairments
of the nervous system such as hemiplegia, ataxia, Parkinson's
disease, and (partial) damage to the spinal cord
(2) For patients with inflamed joints,
hips, broken vertebrae and the like following orthopedic surgery
(3) For patients with respiratory
and circulatory problems who need to improve their heart and lung
functions
(4) For patients weakened by long-term
confinement to their beds
(5) For patients in need of exercise
to combat problems such as diabetes and obesity
Future development goals
Our aim is to improve the system
by adding new video software to encourage continuous exercise
and by developing and enhancing system functionality to satisfy
a wider range of rehabilitation objectives. Furthermore, by combining
the system with vital sign monitors such as electrocardiograms
and blood pressure readings, a further objective can be to improve
load control and enhance the system's safety and scientific validity.
- ### -
|