| |
MITSUBISHI ELECTRIC AND SPC ELECTRONICS
DEVELOP WORLD'S FIRST PROCESS EQUIPMENT FOR REMOVING RESIST IN
LCD MANUFACTURING
Eliminates the need for chemicals and reduces
running costs, environmental impact, and installation space
Tokyo--October 10, 2000--Mitsubishi
Electric Corporation (President and CEO: Ichiro Taniguchi) and SPC
Electronics Corporation (President: Naoki Hashimoto) have jointly
developed resist*1
removal technology using high concentration
ozone, and also single substrate process equipment*2
for removing resist used in the manufacture
of LCDs *3.
Single substrate equipment
for removing resist used in the manufacture of LCDs was developed
using Mitsubishi Electric's high concentration clean ozone generation
technology, technology for high speed removal of resist using ozone,
and SPC's washing equipment technology. It is the first resist removal
equipment in the world that does not use expensive chemicals (resist
removal liquid*4).
This equipment does not use the expensive resist
removal liquid. Consequently, its running cost can be reduced to
1/5 of that of conventional equipment. Furthermore, there is no
need to treat waste water including removal liquid, thus enabling
environmental impact to be reduced to 1/10 or less. In addition,
the use of ozone permits the resist removal process to be integrated
with the substrate washing process that was previously necessary
after the resist was removed, thus enabling installation space to
be reduced by about 1/2. Furthermore, single substrate process equipment
is used by the line conveying method, enabling the equipment to
easily handle large LCD substrates for television sets, and so on.
It is also possible to use this equipment instead of a conventional
types, which use removal liquid, or to use it in combination with
a conventional types.
Development Background
In the manufacture of LCDs, the processes
of pattern fabrication (film deposition, resist coating, exposure,
development, etching, and so on), resist removal, and substrate
washing are repeated several times, then transistors are formed
on the glass substrate. Previously, removal liquid was used in the
resist removal process, and also a combination of ultraviolet light
irradiation and water washing was used for cleaning the substrate
(Fig.1). However, the removal liquid was expensive
(at least several hundred yen per liter), and was used in large
quantities (at least a several hundred cc per 1m2
of the substrate). Consequently, the cost reduction
of removal liquid and the minimization of environmental impact of
waste liquid were important issues.
Ozone is a powerful oxidizing agent. After taking
part in a chemical reaction, it disassociates and reverts to oxygen,
hence it leaves no residue and causes no environmental impact. Experiments
aimed at realizing a resist removal process have been carried out
for some time, however the removal rate was too slow to be practical.
Development Details
Since 1997, Mitsubishi Electric has been
marketing clean type ozonizers that generate ozone at high concentrations
(200 g/Nm3*5)
or higher) with high efficiency. Now, the company has developed
a new resist removal method employing high concentration ozone.
This method can remove resist about 10 times faster and is more
practical than previous ozone methods.
- Development of high-speed resist removal technology
Up to now, research has been carried out on a method of removing
resist by causing it to react with ozone gas at high temperature
over 250°C and also a method of removal by immersing the substrate
in ozone water made by dissolving ozone in pure water. However
when ozone gas is used, the rate of removal of the resist is about
0.01 µm/minute at room temperature, and even when ozonated
water is used, the removal rate is about 0.1 µm/minute.
In other words, the removal rates of these methods are much lower
than that of existing processes using removal liquid (several
µm/minute); hence these methods are impractical.
Mitsubishi Electric has succeeded in raising the resist removal
speed by using ozone gas that has a concentration of 200 g/Nm3
or more. In addition, as a result of performing a detailed study
of the resist removal mechanism, it was found that the resist
undergoes hydrolysis after being oxidized by the ozone. Mitsubishi
Electric therefore investigated several ways of supplying ozone
and water. As a result, they were able to realize a resist removal
rate of about 1 µm/minute or more, which is about 10 times
as high as that obtained using conventional ozone methods.
- Realization of the line conveying method single substrate
process equipment
The developed equipment is a single substrate equipment that
can perform line conveying (Fig.2). Consequently,
it can handle large substrates, enabling it to help reduce the
cost of manufacturing large substrates used for television screens,
and so on. It is also possible to use this equipment in place
of conventional types, which uses removal liquid, or to use it
in combination with conventional types.
- Reduction of running costs, environmental impact and equipment
floor area
Resist can be removed by using ozone gas generated only from the
raw gas (oxygen gas). Consequently, no costly removal liquid is
needed, and the running cost can be reduced to about 1/5 of that
of a conventional method.
In the previous method, organic compounds in waste water mainly
consisted of removal liquid. Since the resist removal process
using ozone requires no removal liquid, the amount of organic
compounds in waste water can be reduced to less than 1/10.
Also, the oxidizing power of ozone enables organic residue on
the substrate to be dissociated by oxidation, and removed. Consequently,
the previous substrate washing process followed by the resist
removal process is no longer needed. This in turn eliminates the
need for washing equipment that uses ultraviolet light, for example,
after the resist has been removed. Consequently, the area of the
equipment can be reduced to about 1/2 of that of previous equipment.
- Resist removal and washing processes that do not involve
the application of physical force
This equipment makes use of the chemical reaction of ozone.
Consequently, the resist removal and substrate washing processes
do not involve the use of physical forces, such as brush cleaning
or ultrasonic power, that are likely to chip the substrate or
damage the wiring. The overall process is therefore highly reliable
and safe.
Future Developments
From November 2000, SPC will start to test samples
from LCD manufacturers. It will also exhibit panels showing the
new resist removal equipment for LCD manufacturing at the LCD/PDP
International 2000 Exhibition between October 25th and
27th, and will commence marketing the new equipment in
January 2001.
In addition to LCD resist removal, Mitsubishi Electric
intends to apply the new technology to semiconductor resist removal
and wafer washing as well.
|
| |
Fig. 2 New Type Resist Removal Equipment
for LCD Manufacturing
NOTES :
*1 Resist : The material necessary
for forming a pattern during the fine etching process and so on.
It is sensitive to light or an electron beam.
*2 Single substrate
equipment : A method in which one substrate is processed at a time.
*3 LCD : Abbreviation
of Liquid Crystal Display.
*4 Resist removal
liquid : An amine-based solvent, such as the 106 liquid (a mixture
of dimethyl sulfoxide and mono-ethanol amine, EKC (a mixture of
hydroxyl amine, diglycol amine and catechol), and so on. It requires
waste liquid treatment.
*5 200 g/Nm3: Indicates
the concentration of ozone. In the standard condition, 200 g of
ozone gas is contained in 1 m3 of gas.
This is the highest level of ozone concentration produced by a commercially
available ozone generator.
# # #
About Mitsubishi Electric Corporation
With more than 75 years of experience in providing
reliable, high-quality products to both corporate clients and general
consumers all over the world, Mitsubishi Electric Corporation (FTSE:
6503q.l) is a recognized world leader in the manufacture, marketing
and sales of electrical and electronic equipment used in information
processing and communications, space development and satellite communications,
consumer electronics, industrial technology, energy, transportation
and construction. With operations in 36 countries, Mitsubishi Electric
Corporation recorded consolidated group sales of over US$35 billion
in the year ended March 31, 2000. Additional information on Mitsubishi
Electric Corporation is available at global.mitsubishielectric.com.
|