Mitsubishi Electric Offers 2.5-Gbps Optical
Transmitter and Receiver Integrated Modules That Comply with
Multi-source Agreement and ITU/SONET Standards
Tokyo - March 7, 2000 - Mitsubishi Electric
today announced a 2.5 gigabit per second (Gbps) optical transmitter
and receiver integrated modules for high-speed fiberoptic data
and telecommunications applications. The transmitter and receiver
integrated modules comply with several International Telecommunications
Union (ITU) and Synchronous Optical Network (SONET) standards
and is ideal for Synchronous Digital Hierarchy (SDH) STM-16 /
SONET OC-48 applications that are 15- to 60-km distances, such
as within metropolitan area networks and transport networks. The
transmitter and receiver integrated modules also comply with a
multi-source agreement between Mitsubishi Electric Corporation,
Alcatel Optronics, Ericsson Components AB, Lucent Technologies,
and Sumitomo Electric Lightwave Corporation.
The transmitter, MF-2500STA, reduces both power
consumption and module size because it contains an uncooled distributed
feedback laser diode (DFB-LD). The receiver, MF-2500SRA or MF-2500SRB,
reduces module size because it contains an embedded phase-locked-loop
(PLL) circuit. In addition, the MF-2500SRB receiver contains an
embedded avalanche photo diode (APD) and a DC-to-DC converter.
The MF-2500SRA receiver complies with ITU S-16.1 and SONET IR-1
standards. The MF-2500SRB receiver complies with ITU L-16.1, L-16.2,
and V-16.2 standards as well as SONET LR-1 and LR-2 standards.
Future plans are to design 2.5-Gbps transmitter and receiver modules
for 120-km and wavelength division multiplexing (WDM) applications.
Under the terms of the multi-source agreement, Mitsubishi
Electric, Alcatel, Ericsson, Lucent, and Sumitomo have initiated
a series of economical, high-performance 2.5-Gbps uncooled laser
transmitter and receiver modules that will continue with future
product offerings. Modules from each company must conform to requirements
specified in the agreement, including package dimensions and pin
functionality, as well as meeting or exceeding specified optical
and electrical characteristics. Although the companies involved
in the agreement work closely to implement best-in-class transmitter
features, each company independently designs, develops, markets,
and distributes its own products.
"By offering 2.5-Gbps transmitter and receiver integrated
modules that meet the requirements of the multi-source agreement,
Mitsubishi is helping to provide designers with a reliable supply
of standardized, low-cost, high-performance transmitters," said
Jim Locke, senior marketing manager for optoelectronic products
at Mitsubishi Electronics America. "This agreement means significant
time and cost savings to system developers, who previously had
to support multiple transmitter configurations in order to benefit
from multiple sources."
Specifications
Transmitters and receivers for the integrated modules
that comply with the following standards have corresponding product
numbers:
Transmitter:
ITU S-16.1/SONET IR-1 - MF-2500STA-002VA ITU L-16.1/
SONET LR-1 - MF-2500STA-003VA ITU L-16.2/ SONET LR-2 - MF-2500STA-XXXXX
(not decided)
Receiver:
ITU S-16.1/SONET IR-1 - MF-2500SRA-002VA
ITU L-16.1/ SONET LR-1 - MF-2500SRB-002VA
ITU L-16.2/ SONET LR-2 - MF-2500SRB-XXXXX (not decided)
The transmitter and receiver integrated modules
have the following specifications at 5-volt operation throughout
a temperature range of -40 to +85 degree Celsius:
Optical transmission range:
S-16.1/IR-1: -4.5 to 0 dBm
L-16.1/LR-1: -1.5 to +3 dBm
L-16.2/LR-2: -1.5 to +3 dBm
Optical receiving range:
S-16.1/IR-1: -18.5 to 0 dBm
L-16.1/LR-1: -27.5 to -8 dBm
L-16.2/LR-2: -28.5 to -8 dBm
Packaging and Availability
The optical transmitter and receiver integrated
modules are available in metal-ceramic packages that fit into
a 35.6-mm x 58.6-mm x 8.9-mm footprint. Samples are available
now, with volume production scheduled for the second quarter of
2000.
# # #
About Mitsubishi Electric Corporation
Mitsubishi Electric Corporation offers a diverse
range of optoelectronic products for SDH, SONET, DWDM, data communication,
FITL, as well as passive optical network systems, test and instrumentation
applications, and CATV distribution. The company markets its optoelectronic
products in North America through the Electronic Device Group
of Mitsubishi Electronics America Inc.
Mitsubishi Electric Corporation and its North American
affiliate, Mitsubishi Electronics America Inc., are world-class
suppliers of semiconductors and electronic products for computers,
communications, industrial, Internet-enabled, automotive, and
visual applications. Mitsubishi combines its systems-level expertise
and high-level silicon process technologies to provide chip, chipset
and system-on-chip solutions. The company is ranked among the
top-tier worldwide semiconductor suppliers and offers an extensive
range of semiconductor and computer system components for the
North American marketplace, including embedded DRAM/flash/SRAM,
ASIC, ASSP, MCU, discrete memory, graphics, microwave/RF, optoelectronic,
storage, and flat-panel display products.
Additional information on the Mitsubishi Electric
Semiconductor Group is available at www.mitsubishichips.com.
Editorial Contacts:
| Mitsubishi Electric Corporation
(Japan):
|
|
Matthew Nicholson
03-3218-2346
Matthew.Nicholson@hq.melco.co.jp
|
Motokazu Isozaki
03-3218-2172
Motokazu.Isozaki@hq.melco.co.jp
|
|