| |
Mitsubishi Electric Developing 10-Gbps
Ethernet Transceiver
That Complies With XENPAK Group Multi-Source Agreement
National Fiber Optic Engineers Conference--BALTIMORE--July
9, 2001--The Electronic Device Group of Mitsubishi Electric
& Electronics USA, Inc., today announced that its parent, Mitsubishi
Electric Corporation, is developing a 10-gigabit Ethernet optical
transceiver module that will comply with specifications defined
by the XENPAK Group Multi-Source Agreement (MSA), which Mitsubishi
Electric joined in May 2001. The transceiver promises to bring
higher bandwidth to the network edge, in anticipation of leading-edge
next-generation switch, router, server, and terminal requirements.
It also combines new levels of performance with the low-cost, ease
of installation, and mass production advantages of Ethernet technology.
An advanced feature of the new technology is a "hot pluggable"
electrical interface for easier installation and configuration.
The MSA is based on the proposed IEEE 802.3ae 10-Gigabit Ethernet
Standard, which specifies uniform form factor, size, optical connector
type, and pinout assignments for 10-gigabit-per-second (10-Gbps)
optical transceivers. The MSA covers all four transceiver
types defined in the proposed standard, including 850-nanometer
(nm) serial, 1310-nm serial, 1310-nm WWDM (wide wavelength division
multiplexing), and 1550-nm serial device types. The MSA also
defines the device size at 36 millimeters (mm) (1.5 inches)
wide, 121 mm (4.8 inches) long, and 17.4 mm (0.7 inches) high, which
enables eight devices to be mounted on typical line cards.
Among the key elements the device will
contain include the XAUI 10-gigabit extended attachment unit interface
for electrical input/output connection and the standard SC duplex
fiberoptic connector for the optical interface. A "hot
pluggable" electrical interface allows all port types to be
interchangeable via a standard front-panel connection, and will
enable extended control and monitoring functionality for controlling
and monitoring the output power of the device.
"Mitsubishi Electric joined and supports
the XENPAK Group MSA and the new IEEE 802.3ae 10-Gigabit Ethernet
Standard because it promises to extend the cost-effectiveness of
Ethernet connectivity to higher bandwidth optical transmissions,"
said Daniel Chen, assistant vice president of optoelectronic and
high-frequency products at Mitsubishi Electric & Electronics
USA, Inc. "Mitsubishi Electric supports standards that
provide new levels of performance and make next-generation network
integration easier for customers. The hot pluggability of
new 10-Gbps optical transceivers will also make it much easier for
customers to install and configure their systems."
Availability
Mitsubishi Electric Corporation's affiliate, Mitsubishi Electric
& Electronics USA, Inc., expects to begin business discussions
on this device with North American customers in the third quarter
of 2001.
About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation offers a diverse range of optoelectronic
products for SDH, SONET, DWDM, data communication, FITL, as well
as passive optical network systems, test and instrumentation applications,
and CATV distribution. The company markets its optoelectronic products
in North America through the Electronic Device Group of Mitsubishi
Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation and its North American affiliate,
Mitsubishi Electric & Electronics USA, Inc., are world-class
suppliers of semiconductors and electronic products for communications,
industrial, Internet-enabled, automotive, and visual applications.
Mitsubishi Electric combines its systems-level expertise and high-level
silicon process technologies to provide chip, chipset and system-on-chip
solutions. The company is ranked among the top-tier worldwide semiconductor
suppliers and offers an extensive range of semiconductor and computer
system components for the North American marketplace, including
embedded DRAM/flash/SRAM, ASIC, ASSP, MCU, discrete memory, graphics,
microwave/RF, optoelectronic, and flat-panel display products.
Additional information on the Mitsubishi Electric Semiconductor
Group is available at http://www.mitsubishichips.com/.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks
of Mitsubishi Electric Corporation in the U.S.A., Japan, and other
countries.
Keywords
Mitsubishi, Ethernet, optical, transceiver, optoelectronic, networking,
10 gigabit.
|