News Releases
 
FOR IMMEDIATE RELEASE  
 

MITSUBISHI ELECTRIC INTEGRATES USB 2.0
FUNCTIONALITY WITH 16-BIT MCU TO OPTIMISE
PORTABLE AUDIO AND INTERNET CONNECTIVITY

SUNNYVALE, Calif. -- June 18, 2002 -- In line with the increased demand for highly functional single-chip Universal Serial Bus (USB) solutions for digital audio applications, the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc., introduced a 16-bit embedded microcontroller (MCU) with full-speed USB functions. The M16C/245 (M30245) integrates high capacity memory and USB 2.0 functionality with an M16C MCU core -- noted for its C language efficiency, fast processing speed, low power consumption, and exceptional EMI/EMS performance -- into a single chip. The device is also capable of performing communication data operation processing and main processing, making it ideal for portable audio applications and high-speed Internet content delivery.

The MCU is the latest addition to Mitsubishi Electric's USB family, and was co-developed by Mitsubishi Electric System LSI Design Corporation in Japan and Mitsubishi Electric's Design Engineering Center, based in North Carolina.

"The USB market is driven by a number of factors: speed, functionality, and due to the demand for smaller portable devices, integration," said Richard Sessions, director of embedded systems at Mitsubishi Electric & Electronics USA, Inc. "By utilizing our extensive design resources in Japan and North America, we have combined our expertise in USB with our industry-leading M16C MCU core to meet customer demand and deliver optimal speed with increased functionality in a single chip."

Using a small, thin 100-pin LQFP package, the device features up to a maximum of nine endpoints. The M16C/245 can perform transfer mode on each endpoint, while not only the buffer size, but also each endpoint on transfer mode can be set optionally. A multi-function serial I/O that can transfer up to 32-bit data has been embedded into two channels, which allows serial sound interface with audio codecs. Additionally, there is a CRC (CRC-CCITT, CRC-16) operations circuit embedded for various memory cards, making it possible to select a generative polynomial best suited for the product application.

Packaging and Availability
Mitsubishi Electric's M16C/245 (M30245) is available in a 100-pin LQFP package. Samples will be available in July 2002, with volume production scheduled for September 2002.

M16C/245 Notable Features
- Shortest command operation time: 62.5 ns (shortest command, f(XIN) = 16 MHz)
- Memory capacity: 128 Kbytes Flash; 10 Kbytes RAM
- Power supply/voltage: 3.0-3.6V (16 MHz)
- USB: USB 2.0 Full Speed specifications, endpoint 0-4 (simultaneous IN/OUT transfer possible for 1-4), FIFO buffer size: 3.25 Kbytes
- Serial I/O: clock synchronization/UART/multi-function S10 x 2, clock synchronization/UART x 2
- 10-bit/8-bit analog-to-digital converter
- 16-bit timers: 5

# # #

About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation is a top-10 semiconductor supplier and ranks among the top-five worldwide suppliers of 8- and 16-bit microcontrollers. The company designs and manufactures powerful embedded MCU platforms for embedded industrial control, automotive, consumer entertainment, and communications applications. Mitsubishi Electric's MCU products include the number one global selling 16-bit, M16C platform -- a feature-rich, low-noise, ultra-low power, and code-efficient core that easily scales across customers' end-product lines. The company also offers 8-, 16-, and 32-bit point solution MCU platforms including USB; Flash-Over-USBTM CAN; LIN; and keyboard, battery, and LCD control.
All Mitsubishi Electric semiconductor global manufacturing facilities, engineering design centers, and marketing and sales centers supplying MCU products to the automotive industry are QS-9000 certified. Mitsubishi Electric is a founding member of EEMBC--the Embedded Microprocessor Benchmark Consortium-and is a member of the USB Implementers Forum and the Smart Battery Implementers Forum. The company markets its microcontroller products in North America through the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric also offers an extensive range of semiconductor and system components for the North American marketplace, including optoelectronic, microwave/RF, ASIC, ASSP, and memory ICs and modules. Additional information on the Mitsubishi Electric Semiconductor Group is available at http://www.mitsubishichips.com/.


Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of Mitsubishi Electric Corporation in the USA, Japan, and other countries. All other companies and products referenced herein are trademarks or registered trademarks of their respective holders.

Keywords
Mitsubishi, M16C, 16-bit, USB, Universal Serial Bus, microcontroller, MCU.

Editorial Contacts:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com

Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com

 
  Return to same year archive