News Releases
 
FOR IMMEDIATE RELEASE  
 

MITSUBISHI ELECTRIC'S PHOTO DETECTORS
COST-EFFECTIVELY MEET LOW-POWER REQUIREMENTS FOR 2.5-GBPS OPTICAL NETWORKS

SUNNYVALE, Calif. -- July 9, 2002 -- In response to the increasingly stringent low power consumption and cost-sensitive requirements of the networking market, the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc., today announced two cost-effective photo detector families for fiber to the home (FTTH) and metropolitan area network (MAN) applications. The PD739C13 Photo Detector family and PD839C4 Avalanche Photo Detector family are each capable of detecting 2.5 gigabit per second (Gbps) optical fiber transmissions using only a 3.3-volt power supply.

The new products serve the needs of a wide range of customers for short- to long-reach applications. The PD739C13 family achieves photo detection by integrating a photodiode (PD) with a transimpedance amplifier (TIA) and is designed for optical transmissions of several kilometers (km) to 30 km. The PD839C4 family integrates an avalanche photodiode (APD) with a transimpedance amplifier for 20-km to 100-km optical applications.

By leveraging existing technologies, the new products ensure high reliability while providing customers with a smooth transition to volume production and a stable source of supply. The new products maintain the same package, pin positioning, and functions as Mitsubishi Electric's 5.0-volt photo detector products, thereby making existing designs easy to upgrade and reducing the time-to-market for next-generation products.

"Mitsubishi Electric's new photo detector families cost-effectively serve a wide range of applications with extremely low power consumption and high reliability," said Daniel Chen, assistant vice president of high-frequency products for Mitsubishi Electric & Electronics USA, Inc. "The families use technology that customers will find familiar, taking much of the guesswork out of next-generation designs while keeping production lines up and running."

Packaging and Availability
Members of Mitsubishi Electric's PD739C13 Photo Detector and PD839C4 Avalanche Photo Detector families are each housed in a 5.6-mm diameter general-purpose package with an attached ball lens.
Samples of both families will be available this month, with volume production scheduled for October 2002.

Key Features
- High sensitivity: PD739C13 = 0.85 amps per watt; PD839C4 = 0.85 amps per watt at a multiplication factor of 1
- High-speed response: PD739C13 = 2 GHz; PD839C4 = 2 GHz at a multiplication factor of 10
- High transimpedance: 1.4 Kohms
- Typical receiver sensitivity: PD739C13 = -23 dBm; PD839C4 = -33 dBm

# # #

About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation offers a diverse range of optoelectronic products for SDH, SONET, CWDM, DWDM, data communication, and FITL applications, as well as passive optical network systems, test and instrumentation applications, and CATV distribution. The company markets its optoelectronic products in North America through the Electronic Device Group of Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation and its North American affiliate, Mitsubishi Electric & Electronics USA, Inc., are world-class suppliers of semiconductors and electronic products for communications, industrial, Internet-enabled, automotive, and visual applications. Mitsubishi Electric combines its systems-level expertise and high-level silicon process technologies to provide chip, chipset, and system-on-chip solutions. The company is ranked among the top-tier worldwide semiconductor suppliers and offers an extensive range of semiconductor and computer system components for the North American marketplace, including DRAM, flash, SRAM, ASIC, ASSP, MCU, microwave/RF, and optoelectronic devices.
Additional information on the Mitsubishi Electric Semiconductor Group is available at http://www.mitsubishichips.com/.

Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of Mitsubishi Electric Corporation in the U.S.A., Japan, and other countries.

Keywords
Mitsubishi, optoelectronic, photo detector, avalanche photo detector, photodiode, avalanche photodiode, transimpedance amplifier, 2.5 Gbps, 2.5 Gb/s, FTTH, fiber to the home, MAN, metropolitan area network, network, short reach, long reach.

Editorial Contacts:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com

Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com

 
  Return to same year archive