| |
MITSUBISHI ELECTRIC'S NEW 32-BIT AUTOMOTIVE MCU OFFERS INDUSTRY'S LARGEST FLASH MEMORY CAPACITY
SUNNYVALE, Calif. -- October 2, 2002 --
The Electronic Device Group of Mitsubishi Electric & Electronics
USA, Inc., furthered its commitment to the North American automotive
market by introducing two M32R/ECU 32-bit microcontrollers designed
for high-end, controller area network (CAN) automotive applications,
such as engine control, airbag system, and EV (motor control), as
a cost-effective, high-performance alternative to microprocessors.
The new devices, dubbed the M32R/ECU#5 (M32180 Group) and M32R/ECU#5HL
(M32182 Group), offer up to 1 Mbyte of flash memory -- the industry's
largest flash capacity -- incorporate a more advanced M32R floating
point unit (FPU) core, boost clock speed up to 80 MHz, and operate
throughout a wide temperature range (-40 to +125 degrees C).
"Mitsubishi Electric's M32R/ECU microcontrollers are an industry
leader in on-chip flash memory capacity, and the latest generation
of devices continues that tradition," said Richard Sessions,
director of embedded systems at Mitsubishi Electric & Electronics
USA, Inc. "Adding the FPU and doubling the processing speed
accelerates performance to a microprocessor level in high-end automotive
systems for a more cost-effective value. Mitsubishi Electric accelerated
the process of debugging code with our new JTAG Interface With Tracing
development tool, so customers can get to market faster."
Powerful M32R-FPU Core
The new generation of devices incorporates an FPU into Mitsubishi
Electric's original compact M32R 32-bit high-performance RISC core.
The new core is fully IEEE 754 compliant for single-precision operations
and supports all exceptions defined in the IEEE 754 specification.
The FPU greatly boosts the operation-speed performance of the new
M32R microcontrollers, reducing single-precision instruction time
by 95 percent and cutting in half the execution time of double-precision
instructions, compared to previous-generation devices. The core
also executes most frequently used instructions in one clock cycle,
as well as compound instructions that execute two operations in
one cycle.
The M32R-FPU core is capable of high code efficiency because its
instruction set accommodates 16-bit and 32-bit instructions. The
FPU incorporates multiply-accumulate and difference-of-products
instructions that are suitable for Fast Fourier Transform (FFT)
butterfly computation, as well as DSP-function instructions for
the built-in multiplier-accumulator.
In addition, the M32R-FPU core supports a wide logical address space
of 4 Gbytes without requiring segment switching, thus resulting
in higher computational efficiency.
Large-Capacity Flash Memory
The new M32R/ECU devices offer large DINOR flash memory capacity
to increase productivity at the development of manufacturing stages,
and to contribute to improved maintainability in the field. The
M32R/ECU#5 offers 1,024 Kbytes of flash memory with 48 Kbytes of
RAM, and the M32R/ECU#5HL offers 384 Kbytes of flash memory and
64 Kbytes of RAM. Both devices offer memory expansion, which allows
designers to add external discrete memory capacity.
Mitsubishi Electric's DINOR flash memory enables customers to program
using a single 3.3- or 5.0-volt power supply. Designers can program
quickly at a rate of 64 Kbytes every two seconds, regardless of
the operating frequency. The devices support serial programming
or software-based CPU programming as well as block erase and collective
erase modes, giving designers more flexibility. The flash memory
even provides a security function that protects against unauthorized
readout or modification by any third party.
JTAG Interface With Tracing Development Tool
The new M32R/ECU devices incorporate a special tracing tool into
the JTAG interface to streamline the code debugging process. The
tool captures many clock cycles of code execution history so that
designers can quickly narrow a coding problem to its source and
make corrections, enabling faster time-to-market development.
Broad Development Tools Support
The M32R/ECU family is supported by proprietary and third-party
development tools, such as system modeling software, real-time operating
systems, C code generators, debugging and data calibration, and
flash programming tools.
Packaging and Availability
Mitsubishi Electric's M32R/ECU#5 microcontroller is available in
a 240-pin QFP package. Samples will be available in June 2003 with
volume production scheduled for March 2004.
The M32R/ECU#5HL microcontroller is available in a 144-pin QFP package.
Samples will be available in February 2003 with volume production
scheduled for September 2003.
# # #
About Mitsubishi Electric & Electronics USA,
Inc.
Mitsubishi Electric Corporation is a top-10 semiconductor supplier
and ranks among the top-five worldwide suppliers of 8- and 16-bit
microcontrollers. The company designs and manufactures powerful
embedded MCU platforms for embedded industrial control, automotive,
consumer entertainment, and communications applications. Mitsubishi
Electrics MCU products include the number one global selling
16-bit, M16C platform -- a feature-rich, low-noise, ultra-low
power, and code-efficient core that easily scales across customers
end-product lines. The company also offers 8-, 16-, and 32-bit point
solution MCU platforms including USB; Flash-Over-USB; CAN;
LIN; and keyboard, battery, and LCD control.
All Mitsubishi Electric semiconductor global manufacturing facilities,
engineering design centers, and marketing and sales centers supplying
MCU products to the automotive industry are QS-9000 certified. Mitsubishi
Electric is a founding member of EEMBC--the Embedded Microprocessor
Benchmark Consortium--and is a member of the USB Implementers
Forum and the Smart Battery Implementers Forum. The company markets
its microcontroller products in North America through the Electronic
Device Group of Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric also offers an extensive range of semiconductor
and system components for the North American marketplace, including
optoelectronic, microwave/RF, ASIC, ASSP, and memory ICs and modules.
Additional information on the Mitsubishi Electric Semiconductor
Group is available at http://www.mitsubishichips.com/.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks
of Mitsubishi Electric Corporation in the USA, Japan, and other
countries. All other companies and products referenced herein are
trademarks or registered trademarks of their respective holders.
Keywords
Mitsubishi, M32R/ECU, M32R, 32-Bit, CAN, microcontroller, MCU.
|
Editorial Contacts:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com
|
|
| |
|