| |
MITSUBISHI ELECTRIC SIMPLIFIES MCU MIGRATION PATH TO MORE
POWERFUL PERFORMANCE WITH NEW ULTRA-POWER-EFFICIENT 16-BIT PLATFORM
MICROCONTROLLER
Platform Design and Flash Reliability
Are Key to Meeting Customer Requirements
SUNNYVALE, Calif. -- October 7, 2002 --
As market migration from 8- to 16-bit microcontrollers (MCUs)
continues to gather pace, the Electronic Device Group of Mitsubishi
Electric & Electronics USA, Inc., launched the M16C/26 (M3026x),
an ultra-low power MCU for powerful, yet power-sensitive applications.
The M16C/26 offers 16-bit peripherals and performance up to 20 megahertz
(MHz) at 8-bit price ranges for consumer, industrial and automotive
control applications. In line with the current easy-to-use, powerful
M16C family of 16-bit platform MCUs, the new flash-based MCU has
high C-code efficiency, excellent EMI/EMS performance, and complete
code and pin compatibility with other M16C Platform MCUs.
The M16C/26 is the first of a new series of MCUs targeting power
management, instrumentation, point-of-sale, remote security, three-phase
motor control, and meter applications where high processing performance,
powerful peripherals, and low power consumption are key factors.
"There is a definite shift occurring right now in the MCU market
to more powerful and flexible processors," said Richard Sessions,
director of embedded systems for Mitsubishi Electric & Electronics
USA, Inc. "Our platform design allows easy and cost-effective
transition to 16-bit performance at 8-bit prices. The M16C/26 offers
highly reliable flash ROM and virtual data EEPROM for applications
that demand performance."
By integrating a sophisticated voltage down converter, the M16C/26
is capable of operating at full rated 20-MHz speed with ultra-low
power consumption across a wide voltage range of 3.0 to 5.5 volts
(10 MHz at under 3.0 volts). This is particularly key for applications
that require high processing capability at low voltages such as
gas, water, and electric meters and remote security systems.
In addition to the migration to more powerful 16-bit processors,
the MCU market is seeing a shift from mask to flash-based MCUs as
flash versions reach value parity and allow much more design flexibility,
which significantly improves product time-to-market.
Mitsubishi Electric's M16C flash MCUs are widely used in many "mission
critical" applications including automotive safety, industrial
control, communications, and computing systems. They use an extremely
robust proprietary Hyper New DINOR flash technology that is not
affected by process variations. This is achieved by creating memory
cells with enough margin in operations and characteristics to eliminate
bit failures and by setting in-process screening steps to remove
defect-induced data retention failures. In addition, all M16C flash
MCUs are capable of 100,000 erase/write cycles (typical).
"With tens of millions of flash devices in service, we have
had no flash ROM bit failures from the field. You can use M16C flash
MCUs in complete confidence, without fear of failure or more expensive
manufacturing due to flash reliability issues," added Sessions.
Packaging and Availability
Mitsubishi Electric's M16C/26 is available in a compact, 7-mm x
7-mm, 48-pin QFP package. Samples of the M16C/26 and StarterKit
Plus development tools are available now, with volume production
scheduled for the first quarter of 2003.
M16C/26 Notable Features
| - |
Operating frequency: 20 MHz at
3.0 to 5.5 volts; 10 MHz at under 3.0 volts |
| - |
Flash memory: 16-, 32-, 48- or 64-Kbytes |
| - |
RAM: 1-, 2-, 4- or 10-Kbytes |
| - |
Virtual EEPROM: 4-Kbytes |
| - |
16-bit timers: 8 |
| - |
Watchdog timer: 1 |
| - |
A/D converter: 10-bit x 8-channel, including
one I2C channel |
| - |
UART: 8-bit x 3-channel |
| - |
Programmable I/O ports: 38 |
| - |
Power supply: 2.7-5.5 volts |
| - |
System clock generator (also includes ring
oscillator) |
| - |
DMA controller: 2-channel |
| - |
Three-phase motor control circuit |
| - |
Brown-out detection circuit |
# # #
About Mitsubishi Electric & Electronics USA,
Inc.
Mitsubishi Electric Corporation is a top-10 semiconductor supplier
and ranks among the top-five worldwide suppliers of 8- and 16-bit
microcontrollers. The company designs and manufactures powerful
embedded MCU platforms for embedded industrial control, automotive,
consumer entertainment, and communications applications. Mitsubishi
Electrics MCU products include the number one global selling
16-bit, M16C platform -- a feature-rich, low-noise, ultra-low
power, and code-efficient core that easily scales across customers
end-product lines. The company also offers 8-, 16-, and 32-bit point
solution MCU platforms including USB; Flash-Over-USB; CAN;
LIN; and keyboard, battery, and LCD control.
All Mitsubishi Electric semiconductor global manufacturing facilities,
engineering design centers, and marketing and sales centers supplying
MCU products to the automotive industry are QS-9000 certified. Mitsubishi
Electric is a founding member of EEMBC--the Embedded Microprocessor
Benchmark Consortium--and is a member of the USB Implementers
Forum and the Smart Battery Implementers Forum. The company markets
its microcontroller products in North America through the Electronic
Device Group of Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric also offers an extensive range of semiconductor
and system components for the North American marketplace, including
optoelectronic, microwave/RF, ASIC, ASSP, and memory ICs and modules.
Additional information on the Mitsubishi Electric Semiconductor
Group is available at http://www.mitsubishichips.com/.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks
of Mitsubishi Electric Corporation in the USA, Japan, and other
countries. All other companies and products referenced herein are
trademarks or registered trademarks of their respective holders.
Keywords
Mitsubishi, M16C, microcontroller, MCU, 16-bit.
|
Editorial Contacts:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com
|
|
| |
|