| |
MITSUBISHI ELECTRIC SAMPLES 40-GBPS EA MODULATOR CHIP AND
MODULE THAT COMBINE INDUSTRY'S HIGHEST INPUT POWER TOLERANCE WITH
LOW CHIRP
Makes 40-km Transmissions Possible for
Next-Generation DWDM Optical Networks
SUNNYVALE, Calif. -- November 18, 2002
-- The Electronic Device Group of Mitsubishi Electric &
Electronics USA, Inc., today announced a 40 gigabit per second (Gbps)
electro-absorption (EA) modulator chip and module that demonstrate
an input power tolerance of up to 15 dBm, the industry's highest,
combined with low chirp[1].
Designed for C Band[2], the devices' high
input power tolerance enables them to offer a significant transmission
distance boost to 40 km without an optical amplifier when using
dispersion-shifted fiber - double the distance of previous-generation
devices. The new EA modulator products represent a significant cost
and space advantage for DWDM[3] applications
compared to lithium-niobate alternatives.
"These EA modulator products represent a significant technological
breakthrough for next-generation optical systems because they combine
high input power capability, intermediate reach, and low chirp,
" said Daniel Chen, assistant vice president of high-frequency
products for Mitsubishi Electric & Electronics USA, Inc. "Their
small package size is an added bonus."
ML9XX38 Chip
Developed using InGaAsP[4] technology,
the ML9XX38 EA modulator chip uses an asymmetric quantum well absorption
layer that is deposited on a semi-insulating indium-phosphide substrate.
This layer prevents degradation of the optical waveform by photocarrier
buildup, which normally occurs when an EA modulator is operated
with high input power. As a result, the ML9XX38 chip attains a high
input power of 15 dBm with a chirp parameter of less than 0.5 (at
-0.5 volts). The chip occupies a tiny 0.3-mm x 0.3-mm footprint,
making module integration easier.
FU-682PEM Module
The FU-682PEM EA modulator module integrates
the ML9XX38 chip and a thermoelectric cooler. The module offers
a high input power tolerance of 13 dBm with a low dispersion penalty
of 2.0 dB (maximum) for 40-km transmissions that use dispersion-shifted
fiber, along with an input impedance of 50 ohms. The module's wide
operating temperature range (0 to +70 degrees C) enables it to operate
in a wide variety of environmental conditions. The FU-682PEM is
housed in a 5-pin V connector package, occupying a 24-mm x 17-mm
x 10-mm footprint, with a PMF[5] pigtail.
Availability
ML9XX38 samples will be available in November 2002, with the volume
production schedule to be determined, based on customer demand.
FU-682PEM samples will be available in December 2002.
# # #
Definitions
[1] chirp = dynamic wavelength drift
[2] C Band = 1530-1565 nm wavelength range
[3] DWDM = dense wavelength division multiplexing
[4] InGaAsP = indium gallium arsenide phosphide
[5] PMF = polarization maintaining fiber
NOTE: A technical paper presentation on the base technology
used in the ML9XX38 chip was presented at the European Conference
on Optical Communication (ECOC 2002) in Copenhagen, Denmark.
About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation offers a diverse range of optoelectronic
products for SDH, SONET, 10GbE, CWDM, DWDM, data communication,
and OTDR applications, as well as passive optical network systems,
test and instrumentation applications, and CATV distribution. The
company's optoelectronic product families conform to leading-edge
current and future multi-source agreements such as XENPAK, X2, and
XFP. Mitsubishi Electric markets its optoelectronic products in
North America through the Electronic Device Group of Mitsubishi
Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation and its North American affiliate,
Mitsubishi Electric & Electronics USA, Inc., are world-class
suppliers of semiconductors and electronic products for communications,
industrial, Internet-enabled, automotive, and visual applications.
Mitsubishi Electric combines its systems-level expertise and high-level
silicon process technologies to provide chip, chipset, and system-on-chip
solutions. The company is ranked among the top-tier worldwide semiconductor
suppliers and offers an extensive range of semiconductor and computer
system components for the North American marketplace, including
microcontroller, ASSP, ASIC, flash, SRAM, DRAM, optoelectronic,
and microwave/RF devices.
Additional information on the Mitsubishi Electric Semiconductor
Group is available at http://www.mitsubishichips.com/.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of
Mitsubishi Electric Corporation in the U.S.A., Japan, and other
countries.
Keywords
Mitsubishi, optoelectronic, electro-absorption modulator, DWDM,
40 Gbps, 40 gigabit.
|
Editorial Contacts:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com
|
Customer Contact:
(408) 774-3189
customerservice@edg.mea.com |
|