| |
MITSUBISHI ELECTRIC'S TUNABLE DISPERSION COMPENSATORS OFFER
WORLD'S BEST OPTICAL SIGNAL RECOVERY PERFORMANCE
FOR HIGH-SPEED, LONG-REACH WDM SYSTEMS
SUNNYVALE, Calif. -- December 10, 2002
-- The Electronic Device Group of Mitsubishi Electric &
Electronics USA, Inc., today announced the availability of the world's
most effective tunable dispersion compensators for countering the
effects of signal degradation prevalent in high-speed, long-reach
WDM[1] optical network systems. Designed
for 40- and 10-Gbps[2] applications, the
devices more than triple the dispersion tuning range of previous-generation
products. They also enable optical network system designers to automatically
adjust the dispersion compensation function for seasonal or daily
temperature fluctuations in already-installed optical fiber. As
a result, the devices drastically reduce required set-up and maintenance
time and eliminate manual tuning of optical network systems.
"Mitsubishi Electric's dispersion compensators make it possible
for optical system designers to quickly tune their systems just
once at installation and adjust optical signals incrementally from
a remote location as the weather changes," said Daniel Chen,
assistant vice president of high-frequency products for Mitsubishi
Electric & Electronics USA, Inc. "This eliminates the aggravation
of manual tuning, saving customers a substantial amount of time
and servicing costs."
Even though WDM optical transmission technology provides one of
the best solutions available for increasing the speed of information
over network systems that feed the Internet, chromatic dispersion[3]
causes the signal to warp and spread out over long distances, thereby
resulting in transmission errors. Using Mitsubishi Electric's FBG[4]
technology and a temperature control mechanism, the FQ-40C dispersion
compensator can tune the optical signal up to 350 ps/nm for 40-Gbps
applications, and the FQ-10E device can tune up to 1,400 ps/nm for
10-Gbps applications. The devices also demonstrate low group delay
ripple and low polarization mode dispersion for high optical signal
quality and feature low insertion loss for high optical power efficiency.
Availability
Samples of the FQ-40C and FQ-10E dispersion compensators will be
available in January 2003, with volume production scheduled for
the third quarter of 2003.
FQ-40C Specifications
| - |
Optical pass bandwidth: >/= 0.2 nm |
| - |
Channel pass bandwidth (-1 dB): >/= 0.6
nm |
| - |
Dispersion tuning range: >/= 350 ps/nm |
| - |
Group delay ripple: </= +/- 2 ps |
| - |
Insertion loss: </= 5 dB |
| - |
Polarization mode dispersion: </= 0.5 ps |
| - |
Power dissipation: 3 watts |
FQ-10E Specifications
| - |
Optical pass bandwidth: >/= 0.2 nm |
| - |
Channel pass bandwidth (-1 dB): >/= 0.3
nm |
| - |
Dispersion tuning range: >/= 1,400 ps/nm |
| - |
Group delay ripple: </= +/- 6 ps |
| - |
Insertion loss: </= 4 dB |
| - |
Polarization mode dispersion: </= 0.5 ps |
| - |
Power dissipation: 3 watts |
# # #
Definitions
[1] WDM - Wavelength Division Multiplexing, which is an information
transmission method that adopts many wavelengths as signal carriers
in a single optical fiber.
[2] Gbps - Gigabit per second
[3] Chromatic dispersion - A phenomena in which optical signal pulses
spread after they travel through installed optical fiber. This signal
spreading occurs because the group velocity depends upon the individual
wavelengths.
[4] FBG - Fiber Bragg Grating
About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation offers a diverse range of optoelectronic
products for SDH, SONET, 10GbE, CWDM, DWDM, data communication,
and OTDR applications, as well as passive optical network systems,
test and instrumentation applications, and CATV distribution. The
company's optoelectronic product families conform to leading-edge
current and future multi-source agreements such as XENPAK, X2, and
XFP. Mitsubishi Electric markets its optoelectronic products in
North America through the Electronic Device Group of Mitsubishi
Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation and its North American affiliate,
Mitsubishi Electric & Electronics USA, Inc., are world-class
suppliers of semiconductors and electronic products for communications,
industrial, Internet-enabled, automotive, and visual applications.
Mitsubishi Electric combines its systems-level expertise and high-level
silicon process technologies to provide chip, chipset, and system-on-chip
solutions. The company is ranked among the top-tier worldwide semiconductor
suppliers and offers an extensive range of semiconductor and computer
system components for the North American marketplace, including
microcontroller, ASSP, ASIC, flash, SRAM, DRAM, optoelectronic,
and microwave/RF devices.
Additional information on the Mitsubishi Electric Semiconductor
Group is available at http://www.mitsubishichips.com/.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of
Mitsubishi Electric Corporation in the U.S.A., Japan, and other
countries.
Keywords
Mitsubishi, optoelectronic, dispersion compensator, 40 Gbps, 40
Gb/s, 10 Gbps, 10 Gb/s.
|
Editorial Contacts:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com
|
Customer Contact:
(408) 774-3189
customerservice@edg.mea.com
|
|