| |
MITSUBISHI ELECTRIC CONTINUES INVESTMENT INTO MOSFET-BASED
SILICON RF PRODUCTS FOR VHF, UHF, AND 800-MHZ APPLICATIONS
New Design Accelerator Kit Radically Improves
Start-Up Time for Radio Designs
SUNNYVALE, Calif. -- February 18, 2003
-- Following the success of its unique Design Accelerator
Kit for its SMD[1] high-power GaAs FETs[2],
the Electronic Device Group of Mitsubishi Electric & Electronics
USA, Inc., today introduced the "Design Accelerator Kit 2"
for its new consolidated line of MOSFET-based silicon RF modules
for VHF and UHF applications. The new Design Accelerator Kit, featuring
Mitsubishi Electric's proprietary DataSurveyor software, enables
designers to review the RA07MxxxxM device family to evaluate the
performance characteristics of each device in a matter of minutes,
rather than weeks, slashing both development costs and time-to-market.
"Just as we addressed the needs of microwave fixed wireless
access designers with our first Design Accelerator Kit, we have
designed our newest kit to help VHF and UHF radio designers avoid
wasting time in the initial design phase," said Bryon Gutow,
senior product marketing manager for microwave and RF products at
Mitsubishi Electric & Electronics USA, Inc. "This kit eliminates
guesswork in selecting a suitable product for the end application,
saving designers up to two weeks in the initial design process.
All designers have to do is attach the connectors, hook up the DC
bias voltage, and begin measuring."
"At a time when many suppliers have abandoned the VHF, UHF,
and 800-MHz radio market, Mitsubishi Electric is investing more
into it," added Gutow. "Our new 'Design Accelerator Kit
2', along with the continued rollout of our new line of MOSFET-based
RF modules and discrete silicon power transistors, demonstrates
that we are committed to providing long-term support for these customers."
Design Accelerator Kit 2 includes DataSurveyor processing software,
a test board (mounted on a heat sink), applications data, and two
samples of each of the following silicon RF modules:
| - |
RA07M1317M-E01 -- 135 MHz to 170 MHz |
| - |
RA07M2127M-E01 -- 215 MHz to 270 MHz |
| - |
RA07M3340M-E01 -- 330 MHz to 400 MHz |
| - |
RA07M4047M-E01 -- 400 MHz to 470 MHz |
| - |
RA07M4452M-E01 -- 440 MHz to 520 MHz |
Availability
The Design Accelerator Kit 2 is available now.
# # #
Definitions
[1] SMD -- surface mount device
[2] GaAs FET -- gallium arsenide field effect transistor
About Mitsubishi Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation manufactures a diverse range
of microwave and RF semiconductors for linear, low-noise, and high-power
communications applications, including satellite and terrestrial
transmitters and receivers, mobile radios, cellular phones, and
subscriber units. The company produces gallium-arsenide (GaAs) FETs,
modules, and MMICs using HBT, PHEMT, MESFET, HEMT, and HFET technologies.
The company also produces silicon RF power transistors and modules
using MOS and LDMOS technologies for the industrial and consumer
markets. Mitsubishi Electric markets its microwave and RF semiconductors
in North America through the Electronic Device Group of Mitsubishi
Electric & Electronics USA, Inc.
Mitsubishi Electric Corporation and its North American affiliate,
Mitsubishi Electric & Electronics USA, Inc., are world-class
suppliers of semiconductors and electronic products for communications,
industrial, Internet-enabled, automotive, and visual applications.
Mitsubishi Electric combines its systems-level expertise and high-level
silicon process technologies to provide chip, chipset, and system-on-chip
solutions. The company is ranked among the top-tier worldwide semiconductor
suppliers and offers an extensive range of semiconductor and computer
system components for the North American marketplace, including
DRAM, flash, SRAM, ASIC, ASSP, MCU, microwave/RF, and optoelectronic
devices.
Additional information on the Mitsubishi Electric Semiconductor
Group is available at www.mitsubishichips.com.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks
of Mitsubishi Electric Corporation in the USA, Japan, and other
countries. DataSurveyor is a trademark of Mitsubishi Electric &
Electronics USA, Inc. All other companies and products referenced
herein are trademarks or registered trademarks of their respective
holders.
Keywords
Mitsubishi, Design Accelerator Kit, DataSurveyor, RF modules, RF
transistors, microwave, radio, VHF, UHF, 800 MHz.
|
Editorial Contacts:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com
|
Customer Contact:
(408) 774-3189
customerservice@edg.mea.com |
|