| |
MITSUBISHI ELECTRIC LAUNCHES 350-MHZ, 18-MBIT NETWORK SRAM
WITH ULTRA-WIDE 72-BIT BUS
SigmaRAM Device's Density Scalability
Decreases Redesign Costs
SUNNYVALE, Calif. -- February 25, 2003 --
As industry-wide adoption of broadband connectivity continues,
the Electronic Device Group of Mitsubishi Electric & Electronics
USA, Inc., today announced an 18-megabit (Mbit) SigmaRAM Network
SRAM that achieves a 350-MHz clock speed and offers a 72-bit bus
width. The new double-late-write device offers 100 percent data-bus
efficiency and an exceptionally fast data throughput of 25 gigabits
per second, making it an ideal choice for broadband networking and
telecommunications system applications, such as routers and switches.
"Telecom engineers and network designers are always looking
to push the envelope when it comes to data throughput, but not compromise
on space and power consumption," said Tad Keeley, senior product
marketing manager for SRAMs at Mitsubishi Electric & Electronics
USA, Inc. "Operating at a fast clock speed across a wide bus,
this new Network SRAM achieves a higher data throughput than competing
products. In addition, this chip offers all the benefits of the
SigmaRAM architecture, including easy scalability, low EMI, and
lower system cost."
The SigmaRAM architecture presents an open set of standards that
deliver very fast clock speeds, exceptionally quick access times,
high density, outstanding noise immunity, and extremely wide buses.
The architecture also offers memory scaling using the same package
in future product generations. Customers can incorporate the 18-Mbit
device in an existing design, then replace it with a 36-Mbit, 72-Mbit,
or 144-Mbit device without expensive redesign, enabling future products
to come to market quicker and more cost-effectively.
"This new chip shows Mitsubishi Electric's continued commitment
to bring high-quality products to market that mirror the needs of
our customers," added Keeley. "We continue to expand our
Network SRAM product portfolio to give system designers a complete
choice, no matter what memory challenge they are facing."
The new 350-MHz SigmaRAM device is available in both 72-bit-wide
(M5M5Y5672TG) and 36-bit-wide (M5M5Y5636TG) configurations, operating
with a 1.8-volt power supply to offer low power consumption at the
fastest speeds. The devices conform to the SigmaRAM Consortium's
1x1Dp double-late-write,
pipeline-read specification, which enables 100 percent data bus
efficiency and avoids data bus collision even in read/write alternate
operation. Devices conforming to the SigmaRAM 1x1Lp
late-write, pipeline-read specification are also available in both
72-bit-wide (M5M5Y5972TG) and 36-bit-wide (M5M5Y5936TG) configurations.
Packaging and Availability
Mitsubishi Electric's SigmaRAM devices are housed in a 209-ball
BGA package with a 14-mm x 22-mm footprint and a 1-mm ball pitch.
Samples are available now, with volume production scheduled for
April 2003.
Key Features of M5M5Y5672TG Device:
| - |
350-MHz clock speed (2.0-ns
access time) |
| - |
72-bit-wide data bus --
Common I/O |
| - |
Single 1.8-volt power
supply |
| - |
209-ball BGA package |
| - |
Echo clock function available |
Additional Network SRAMs Available:
| - |
M5M5T5672TG -- 200-MHz, 72-bit bus, 2.5-volt
supply, 209-ball BGA package. |
| - |
M5M5T5636UG -- 250-MHz, 36-bit bus, 2.5-volt
supply, 165-ball BGA package. |
| - |
M5M5T5636GP -- 200-MHz, 36-bit bus, 2.5-volt
supply, 100-pin TQFP package. |
| - |
M5M5V5636GP -- 167-MHz, 36-bit bus, 3.3-volt
supply, 100-pin TQFP package. |
# # #
About Mitsubishi Electric & Electronics
USA, Inc.
A top-tier semiconductor supplier, Mitsubishi Electric Corporation
offers a broad range of memory products, such as DRAM, SRAM, and
flash memory as well as an extensive range of other semiconductors.
The company offers its semiconductors in North America through the
Electronic Device Group of Mitsubishi Electric & Electronics
USA, Inc. Additional information on the Mitsubishi Electric Semiconductor
Group is available at http://www.mitsubishichips.com/.
Mitsubishi Electric Corporation and its North American affiliate,
Mitsubishi Electric & Electronics USA, Inc., are world-class
suppliers of semiconductors and electronic products for communications,
industrial, Internet-enabled, automotive, and visual applications.
Mitsubishi combines its systems-level expertise and high-level silicon
process technologies to provide chip, chipset and system-on-chip
solutions. The company is ranked among the top-tier worldwide semiconductor
suppliers and offers an extensive range of semiconductor and computer
system components for the North American marketplace, including
DRAM, flash, SRAM, ASIC, ASSP, MCU, microwave/RF, and optoelectronic
devices.
Additional information on the Mitsubishi Electric Semiconductor
Group is available at http://www.mitsubishichips.com.
About SigmaRAM
The SigmaRAM SRAM architecture is a set of open standards for powerful,
high-speed SRAM devices that are targeted specifically for the networking
and communications markets. Developed through the collaboration
of several leading SRAM companies and approved by JEDEC, the architecture
enables all SRAM manufacturers to develop compatible devices based
on the same specifications.
Trademark Information
Mitsubishi and the Mitsubishi logo are registered trademarks of Mitsubishi Electric Corporation in the USA, Japan, and other countries. SigmaRAM is a trademark of the SigmaRAM Consortium. All other companies and products referenced herein are trademarks or registered trademarks of their respective holders.
Keywords
Mitsubishi, SRAM, SigmaRAM, Network SRAM, networking, communications, telecom, telecommunications.
|
Editorial Contacts:
Positio Investor & Public Relations
Dave Richardson
(650) 815-1006, Ext. 108
dave@positiopr.com
Mitsubishi Electric & Electronics USA, Inc.
John Garner
(408) 774-3191
garner_john@edg.mea.com
|
Customer Contact:
(408) 774-3189
customerservice@edg.mea.com |
|