| |
"GMPLS SIGNALING PROTOCOL INTEROPERABILITY TEST IN MULTILAYER
NETWORK"
--Establishing a Global Standard
for the Next-Generation Photonic Network--
Nippon Telegraph and Telephone Corporation
NEC Corporation
Fujitsu Laboratories Ltd.
The Furukawa Electric Co., Ltd.
Mitsubishi Electric Corporation
Nippon Telegraph and Telephone Corporation (NTT;
Head Office: Chiyoda-ku, Tokyo; President: Norio Wada), NEC Corporation
(Office: Minato-ku Tokyo; President: Akinobu Kanasugi), Fujitsu
Laboratories Ltd. (Office: Kawasaki-shi; President: Michio Fujisaki),
The Furukawa Electric Co., Ltd. (Office: Chiyoda-ku; President:
Junnosuke Furukawa), and Mitsubishi Electric Corporation (President
& CEO: Tamotsu Nomakuchi) are pleased to announce the successful
conclusion to the world's first GMPLS(*1) signaling(*2) interoperability
test using a multilayer network consisting of packet, TDM(*3), wavelength,
and fiber layers. Given the quality requirements set by the application
or traffic state, it is possible to select the optimal communication
path from among all possible paths that can be established on the
multilayer network.
The results of this experiment will be reported on May 22, 2003
in the Workshop held in Kagoshima University organized by the Technical
Group on Photonic-Network-based Internet (PNI) and the Technical
Group of Photonic Switching (PS) in IEICE (The Institute of Electronics,
Information, and Communication Engineering).
Backgrounds and Achievements
GMPLS is a technology that enables unified control management of
the network layers (packet / TDM / wavelength / optical fiber).
In the conventional network, each layer network, such as packets
(like IP), TDM, and wavelength is independently built. Conventional
technology demands that each network layer be independently controlled
by operators who specialize in the corresponding network layer.
For example, in the conventional electric or optical cross-connect,
the network operator administers the terminal of the centralized
control device. This device issues instructions to control cross-connect
equipment and thus the setup of TDM or wavelength paths. When the
cross-connect equipment supports GMPLS control, path setup is established
by exchanging control packets between these control devices as well
as MPLS routers. Therefore, network operator who has MPLS expertise
can manage cross-connects. However, present equipment that supports
GMPLS control simply offers a unified management approach. Each
layer network (IP, TDM, or wavelength) must still be managed separately
as before. It is impossible to handle all layers in the whole network
systematically, such as one side routing using TDM paths where the
other side routing uses wavelength paths.
In order to avoid this problem, control software programs for setting
up and releasing paths in the multilayer network were newly developed
and mounted into the network control devices of each company. The
fact that these control devices can be mutually interconnected is
a key factor in the success of the interoperability test that examined
path setup of multilayer signaling; a world first. These control
devices exchange signals based on protocol of RSVP-TE (*4) extended
to GMPLS to set up and release multilayer paths on the multilayer
network.
The setup examined the test is shown in Figure. This setup was designed
to replicate a multilayer network with various kinds of network
equipment including packet routers, electrical-connects, optical
cross-connects, and optical switch for fiber port switching. It
provides control functionality for both packet paths and TDM paths
using control devices 1 and 2. Control device 1 can freely set the
packet path of route A, and the TDM path of route B. Control device
2 on Route A has path control functions for both packet and wavelength
paths. Control devices 2-6 are for optical cross-connect control,
by which the paths of wavelength are set up. They newly set up a
wavelength path for the packet path from 1 to 7. Thus, the setup
and release of a multilayer path can be performed by exchanging
a control signal between each control device handling a different
layer. Given the quality requirements set by the application or
traffic state, it is possible to select the optimal communication
path from among all possible paths that can be established on the
multilayer network.
Due to the use of GMPLS, network operation can be unified. Significant
reductions in network operation cost can be expected because the
most economic path can be selected by configuring the optimal configuration
of network resource from among all layers of the network. In addition,
novel network services can be created, such as the wavelength-dedicated
line which changes wavelength path connection points according to
user demand. For this reason, GMPLS has been attracting attention
as the base technology of the next-generation broadband IP network.
GMPLS is being actively discussed and advanced in international
standardization organizations, such as IETF (Internet Engineering
Task Force), OIF (Optical Internetworking Forum), and ITU (International
Telecommunication Union).
A future plan
This interoperability test was carried out by the Photonic Internet
Lab (PIL) (*5), which was founded in order to promote research on
and development of the next-generation photonic network(*6)as well
as encouraging global standardization activities. PIL was founded
in September 2002. At present, PIL consists of seven companies;
Oki Electric Industry Co., Ltd. and Hitachi, Ltd. are additions
to the five above-mentioned companies. PIL has two objects: one
is to create new control technologies that can be accepted as international
standards. The second to rigorously test the protocol software code
developed by each company. We are planning to conduct interoperability
tests with a number of global companies.
>>>
Figure. Setup of GMPLS signaling experiment in multilayer network
<Glossary>
 |
 |
 |
| *1 |
GMPLS(Generalized Multi-Protocol Label Switching): |
|
|
| |
GMPLS is a protocol that establishes generalized
MPLS into all layers of the IP network: layer 2, TDM (Time Division
Multiplexing), wavelength (WDM), and the fiber. The basic MPLS
is a control mechanism that attaches fixed length labels to
IP packets. GMPLS is attracting attention for controlling the
next-generation photonic network. Standardization of GMPLS is
being advanced mainly by IETF (The Internet Engineering Task
Force). The basic function of GMPLS was released as a Proposed
Standard in February 2003, with registration number RFC 3471-3473.
In order to make it complete and a truly practical protocol,
world-wide efforts are needed elaborate the remaining details
and develop protocol code that can be directly installed in
network equipment. |
|
 |
|
|
| *2 |
Signaling: |
|
| |
Operation which exchanges signals between the
control devices of network equipment, such as routers and optical
crossing connects in order to set up and release paths. The
format of the control signal and the procedure to exchange control
packets are defined in the signaling protocol. |
|
 |
|
|
| *3 |
TDM (Time Division Multiplexing): |
|
| |
Transmitting technology using time division
multiplexing. SDH/SONET is used widely in many networks. |
|
 |
|
|
| *4 |
RSVP-TE(Resource ReSerVation Protocol with
Traffic Extensions): |
|
| |
One of the protocols for signaling ,that is,
to setup a path and release it. Extended for MPLS from RSVP.
The original RSVP is a protocol for bandwidth reservation. |
|
 |
|
|
| *5 |
Photonic Internet Lab: |
|
| |
Photonic Internet Lab (PIL) is promoting research
into and development of next-generation photonic network technologies
(See http//www.jk.ws32.arena.ne.jp). PIL encourages the submission
of proposals from its members to global standardization bodies,
like ITU-T, IETF, and OIF. PIL also tests the photonic network
control programs developed by PIL member companies.
PIL activities are supported by the R&D support scheme of
the MPHPT (Ministry of Public Management, Home Affairs, Posts
and Telecommunications) for funding selected IT activities. |
|
 |
|
|
| *6 |
Next-generation photonic network: |
|
| |
A network that more fully realizes the benefits
of optical technology; like optical fiber transmission, wavelength
division multiplexing, and so on. At present, optical fiber
and wavelength multiplexing are mainly used for point to point
transmission. The next-generation photonic network demands effective
optical switching technology. Most current switches are electrical
because the few existing optical switches offer insufficient
performance. A high-speed and large-scale network can be created
if advanced optical switching technology (the optical signal
is switched without optical-electrical conversion) can be realized. |
|
For further information, please contact:
|
Minako Sawaki, Hirofumi Motai
Planning Division
NTT Science and Core Technology Laboratory Group
Tel: +81-46-240-5152
E-mail: st-josen@tamail.rdc.ntt.co.jp
Chris Shimizu
NEC Corporation
Tel: +81-3-3798-6511
E-mail:yc-shimizu@cb.jp.nec.com
Network Architecture Laboratory
Network Systems Laboratories
Fujitsu Laboratories Ltd.
Tel: +81-44-754-2765
E-mail: gmpls@ml.labs.fujitsu.com
Nobuyuki Kishi, Osamu Suzuki
Public Relations Section
The Furukawa Electric Co.,Ltd.
TEL: +81-3-3286-3050
E-mail: pub@ho.furukawa.co.jp
Robert Barz
Public Relations Department
Mitsubishi Electric Corporation
TEL: +81-3-3218-2346
E-mail: robert.barz@hq.melco.co.jp
|
|
|
 |