|
 |
Building Systems
Communication Systems
Industrial Automation
Energy & Environment
Semiconductors & Devices
Transportation
Visual Information Systems
 |
 |
 |
MMIC |
 |
 |
Meet the smallest MMIC chip set ever developed, with a built-in power amplifier, low noise amplifier and phase shifters.
The result of our space systems development endeavors, it greatly reduces the operational cost of Active Phased Array Antennas (APAA), as the amplifiers have temperature compensation circuits and do not require external parts such as capacitors or a bias circuit for bias tuning, and the phase shifters are capable of especially high performance.
APAAs, which use fast beam scanning to simultaneously track Quasi-Zenith
satellites as they speed through space, perform well but are expensive due to the large number of expensive microwave circuits required for each antenna. This futuristic tiny new MMIC chip set is making that a thing of the past.
|
|
|
 |