NAYUTA TELESCOPE Mitsubishi Electric Astronomical Observation Technology
Click here to experience the stars...
luminary01 luminary03 luminary05 luminary07 luminary09
luminary02 luminary04 luminary06 luminary08 luminary10
How images reach our eyes Collecting light


To understand how NAYUTA collects light, we must first take a look at the basic mechanism of a reflector telescope.

The surface of the primary mirror is slightly parabolic in order to gather light at a single point. An observation instrument may be placed here, but by attaching a secondary mirror instead, the gathered light is allowed to return to the precise center of the parabolic primary mirror. In this case, the observation instrument is attached to the back side of the primary mirror.

This combination of primary and secondary mirrors also allows the total length of the telescope to be short, and is commonly employed in medium- and large-scale reflector telescopes.

In addition to these two mirrors, NAYUTA has a third mirror that plays a critical role.

Next


How NAYUTA "sees"
How images reach our eyes
What NAYUTA can see
How NAYUTA works
The creation of NAYUTA
NAYUTA telescope performance
Major telescopes built by Mitsubishi Electric
FAQ