NAYUTA TELESCOPE Mitsubishi Electric Astronomical Observation Technology
Click here to experience the stars...
luminary01 luminary03 luminary05 luminary07 luminary09
luminary02 luminary04 luminary06 luminary08 luminary10
How NAYUTA "sees" Precision to 0.00000001%


The performance of a telescope is generally determined by its resolving power and light-gathering power. Resolving power is the ability to distinguish minute objects, and light-gathering power is the ability to gather light. In the case of a reflector telescope, these two factors are greatly affected by the accuracy of the primary mirror.

NAYUTA's primary mirror is two meters in diameter, and is Japan's largest, as well as the world's largest mirror attached to a ground-based telescope. The surface of the mirror is polished to extreme accuracy. In a matter of speaking, it is about the same as leveling a huge baseball field to an accuracy of two microns (1/30th of a strand of hair). Such precision is what it takes to achieve superior performance.


Presition that's almost the same as leveling the vast terrain of Australia to an accuracy equal to the height of a credit card
How NAYUTA "sees"
How images reach our eyes
What NAYUTA can see
How NAYUTA works
The creation of NAYUTA
NAYUTA telescope performance
Major telescopes built by Mitsubishi Electric
FAQ